Release Notes
Version 1.2.0
Added
Master Setup Assistant
BNIs that are to be used in the ADP must be actively selected at the start. Only selected BNIs are configured. Selected BNIs can also be deleted again.
Connection to the Balluff Update Platform
With an active internet connection, ADP Edge updates can be downloaded directly via the WebUI
ADP Cloud: New Guided Changeover Module
Improvements
Changed discovery protocol from TMG UDP to CIP & DCP (→ firewall must be deactivated for UDP ephemeral ports 1024 to 65535)
Default WebUI credentials: user: admin, pw: Balluff#1
No more login necessary when starting ADP for the very first time
Optimize parameter loading
Use volume mapping to store persistent edgenode data
Update ADP edgenode and ADP Cloud modules version to 3.0
Update InfluxDB to latest version
Optimize start up WebUI behaviour
ADP Cloud:
CMTK module has TLS option
BNI module: module requires only one input, which can be copied via the copy button next to the process data
Version 1.3.0
Added
Support of BNI00HM (FW 4.9.1) and BNI00HL (FW 1.3.0)
Read only support for BNIs connected to PLCs
Discovery interface configuration
The interface on which the ADP searches for BNISs can now be specified by users
Enhanced security with HTTPS support
HTTPS is available via port 9999, while the HTTP option remains accessible on port 8888
MQTT enhancements with TLS support
Standard MQTT is available on port 1833, while MQTT over TLS can be accessed through port 8883
Removed Grafana and InfluxDB
Product name of the BNI is displayed in the WebUI now
Added an alert in the WebUI to inform users when a connection to the EdgeNode cannot be established
ADP API layer authentication implemented
Improvements
IO-Link parameters are no longer read out cyclically but by manual triggering
New badge on menu icon to notify users of new BNIs or available updates
Update ADP edgenode and ADP Cloud modules version to 3.1.2
ADP Cloud:
Smartlight module: extend flexi-mode with color selection
GCS module: support of GCS Version 1.7
CMTK module: support of CMTK version 2.0
Back to top