EtherCAT integration

With the EtherCAT integration, the system is made up of the following components:

  • Bus master

  • Bus modules/slaves (here the bus module BNI)

Device data

In order to properly parameterize the bus master, device data in the form of three ESI files is enclosed with the bus module BNI.

Input/output buffer

The data exchange with the controlling system takes place in the input and output buffer. The size of this buffer must be configured by the master.

Configuration

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

During the project planning the BNI bus module is displayed as a modular device. The device data required for the project planning is stored in the ESI files. The data modules of the inputs/outputs, the IO-Link Port and any additional modules are shown in the project planning software in relation to the slot.

The ESI files make available the possible data modules (inputs/outputs, IO-Link Ports of varying data width and other additional modules).

The appropriate data modules are assigned to a certain slot for the configuration of the BNI. Unused slots can be released.

Integration in project planning software

As an example, the connection of the BNI to a Beckhoff TwinCAT control is shown with the TwinCAT System Manager. The exact procedure depends on the project planning software used.

Installing ESI files

The device description has the following name: Balluff BNI XG5-538-1B5-Z067 ECS V.x.x.x.xml

  • Copy the file to the corresponding TwinCAT directory (in the standard: C:\TwinCAT\3.1\Config\Io\EtherCAT).

    ⇒ Installed devices are available when the TwinCAT System Manager starts again.

Automatic scanning

Prerequisite

Before connecting devices to the EtherCAT network, the EtherCAT system must be in a secure, de-energized state.

  1. Switch on the operating voltage and start the TwinCAT System Manager in Config mode.

  2. Scan BNI as a box.

    ../../_images/Automatisch_Scannen.png

    Automatic scanning

Manually adding a device

Prerequisite

Before connecting devices to the EtherCAT network, the EtherCAT system must be in a secure, de-energized state.

  1. Switch on the operating voltage and start the TwinCAT System Manager in Config mode.

  2. Attach a box.

    ../../_images/Geraet_manuell_anfuegen.png

    Manually adding a device

  3. Select a box.

    ../../_images/Box_waehlen.png

    Select a box

Necessary configuration of device

After automatic scanning or manual adding of the device, the device appears in the tree structure of TwinCAT.

../../_images/Geraet_in_Baumstruktur.png

Device in tree structure

The BNI supports EoE (Ethernet over Ethercat). In order to configure TwinCAT, in the EtherCAT tab select Advanced settings.

A valid DNS name and then a valid IP address must be entered.

../../_images/EoE-Konfiguration.png

EoE configuration

Configuring Station Alias

The Station Alias can be selected under the EtherCAT tabAdvanced settings.

  1. Open ESC Access.

  2. Open E²PROM.

  3. Select Configured Station.

    ../../_images/Station_Alias.png

    Configuring Station Alias

Note

The new value is only valid after a reset.

Configuring the network module

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

The BNI is a modular EtherCAT device. The device has the following slot structure:

Data configuration

Slot number

Meaning

1-8

IO-Link Ports

Note

The sum of the output data may not exceed 256 bytes.

../../_images/IO-Link-Modul_konfigurieren.png

Configuring the network module

In order to configure the IO-Link Ports, a defined number of process data (buffer size) must be assigned to the EtherCAT slots. In the TwinCAT System Manager this works as follows:

  1. Delete assignment of IO-Link channel (or port) with x.

  2. Place the channel selected on the left side with with < the module configuration selected on the right.

  3. Transfer configuration to the EtherCAT slave with restart of TwinCAT in Config mode.

Bitmapping and function

Signals from configured inputs or outputs are displayed in the modulesSTD_IN_1bit(inputs Pin 4), Input Pin 2 (inputs Pin 2), as well asSTD_OUT_1bit(outputs Pin 4) and Output Pin 2 (outputs Pin 2).

Note

XG1 devices have no outputs to Pin 2.

Network modules

The IO-Link modules are always established according to the same schema:

IOLI/Ox/xBytes

  • Quantity of process data used (should be greater than or equal to the process data length of the O-Link device)

  • I = Input data

  • O = Output data

  • I/O = Input and output data

Short circuits and restart bits

The BNI restarts automatically if a short circuit occurs at one of the IO-Link Ports. No restart bits are required.

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

In the IO-Link state the current status of each port is displayed.

IO-Link state

Value

Status

0x_0

Port disabled

0x_3

Port in communication OP

0x_4

Port in communication COMSTOP

0x1_

Watchdog detected

0x2_

Internal Error

0x3_

Invalid Device ID

0x4_

Invalid Vendor ID

0x5_

Invalid IO-Link Version

0x7_

Invalid Cycle Time

0x8_

Invalid PD in length

0x9_

Invalid PD out length

0xA_

No device detected

0x0_

No error

0xD_

Voltage low

0xE_

Short circuit

0xF_

Unspecific error

Start-up

In the start-up the IO-Link Ports and outputs can be preconfigured. For more information, see Configuration without ESI.

The entries are transferred during the transfer of the configuration.

../../_images/Startup.png

Start-up

Configuration of modules

../../_images/Konfiguration_der_Module.png

Configuration of modules

Validation

No validation: Validation deactivated, every device is accepted.

Compatibility: Manufacturer ID and device ID are compared with the module data. IO-Link communication is only started if they match.

The following values are possible for the validation setting:

Values for the validation

Value

Validation

0

No validation

1

Compatible (VID + DID)

The validation can be activated via the CoE object additional IO-Link Configuration Data for each port with subindex 1 (validation and backup). The values used for the validation must be configured in the CoE object IO-Link Configuration Data for each port.

Parameter server

Switched on : Data retention functions active, parameter data and identification data of the IO-Link device are saved in a remanent memory.

Disabled : Data storage function disabled, stored data remains stored.

Deleted : Data storage function disabled, stored data is deleted.

Upload enabled : Can be used to select whether an upload of the parameter data to the data storage of the network module port should be performed or not. If the upload is enabled, as soon as a device has requested an upload (Upload flag set) or if no data is saved in the master port (e.g. after deletion of the data or before the first data upload), the master starts uploading the parameter data.

Block upload : No data upload is started if the upload is blocked. For an upload request from the IO-Link device, a download (if activated) is started in the case of different parameter sets as no upload may be carried out.

Enable download : Can be used to select whether a download of the parameter data to the IO-Link device should be performed or not. As soon as the stored parameter data in the port’s parameter server differs from the connected IO-Link device and there are no upload requests from the IO-Link device, a download is performed.

Block download : If the download is blocked, an upload (if activated) of the parameter data takes place, irrespective of the upload flag of the IO-Link device.

Block upload and download : There is no exchange of parameter data if both upload and download are blocked. The IO-Link device communicates then with the IO-Link Port.

The following values are possible for the settings:

Value

Function

0x8X

switch on

0x0X

switch off

0x40

delete

0xX1

Switch on upload

0xX2

Switch on download

The data memory can be activated via the CoE object additional IO-Link Configuration Datafor each port with subindex 1 (validation and backup). There is no read or write access to the content of the data memory via EtherCat.

Note

After uploading the parameter data, the Vendor ID and Device ID of the connected IO-Link device remain stored until the data records are deleted.

Validation takes place when the connected IO-Link device is started up. Only an IO-Link device of the same type can be used for data storage.

In order to use a different type of IO-Link device, the content of the parameter server must be deleted.

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

The upload flag is required in order to overwrite data already saved in the parameter server with new parameter data of the same IO-Link device.

In order to activate the upload flag of an IO-Link device, the value 0x05 must be entered in the parameterIndex 0x02, Subindex 0.

Failsafe values

If the EtherCAT connection fails or if the EtherCAT status is notOperate, the IO-Link Ports use these values:

  • If a port is in the IO-Link stateOperate, the process data displayed is switched to invalid.

  • If Pin 2 or Pin 4 are in the digital output mode, zero (low level) is displayed.

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

Via the object 0x4000 (IO-Link Service Data Ch. X), IO-Link ISDU parameters can be read or written from the IO-Link device. For this purpose, the corresponding index and subindex must be entered and for writing the corresponding length and data must be entered. The read or write operation is started via the control object. The result is displayed in the status object.

Values for the control

Values for the control

Value

Function

0x00

No function

0x02

Write

0x03

Read

Values for the status

Values for the status

Value

Status

0x00

No status

0x01

Active/Busy

0x02

Access

0x04

Error

0xFF

Fail

Example of CoE setting

This example shows how the index 0x40 of Smartlight (mode) is changed by reading and writing.

  1. Select module.

  2. Open CoE - Online.

  3. Activate the setting Auto Update.

  4. Under Advanced select the setting Online - via SDO Information.

    ../../_images/Einstellungen_aktivieren.png

    Activate settings

  5. In port, select 4030:0(here channel 4).

  6. Read index by double clicking 4030:0 and specifying the respective index (here 0x0040 64).

  7. In control write the command 0x03.

    ../../_images/Lesen.png

    Read

    ⇒ Content of the index is read and displayed in data.

  8. Change data, specify length and use the command 0x02.

    ../../_images/Schreiben.png

    ⇒ The data is written and the parameter is changed in the device.

Acyclic access via AoE

The ETG5001.6220 describes AoE instead of CoE for the ISDU read/write access to IO-Link device parameters. Details on ADS can be found in the Beckhoff TwinCAT documentation and in ETG.1020. In contrast to CoE, AoE permits non-blocking processing.

AoE ISDU access uses these definitions (all are 32 bit):

  • AoE IndexGroup = 0x0000F302

  • AoE PortNumber = 0x00001000 + IO-Link port number, starting with 0.

  • AoE IndexOffset

    • 16 Bit IO-Link Index

    • 8 Bit always zero

    • 8 Bit IO-Link Subindex

  • Return error code

    • 16 Bit additional information about the error code, which is 0x0700 (ADS device error).

    • 16 Bit error code via IO-Link

Function blocks ADSREAD and ADSWRITE

../../_images/Funktionsbloecke_ADSREAD_und_ADSWRITE.png

Function blocks ADSREAD and ADSWRITE

Function block ADSREAD in TwinCat

../../_images/Funktionsblock_ADSREAD_DE.png

TwinCat – ADSREAD

ADSREAD commands

Name

Type

Inherited from

Address

Initial

Comment

NETID

T_AmsNetId

Ams net id

PORT

T_AmsPort

ADS communication port

IDXGRP

UDINT

Index group

IDXOFFS

UDINT

IndexOffset

LEN

UDINT

Maximum number of the data bytes to be read (LEN ≤ maximum size of target buffer)

DESTADDR

PVOID

Indicator of target buffer

READ

BOOL

Rising edge starts command execution.

TMOUT

TIME

DEFAULT_ADS_TIMEOUT

Maximum permissible time for the execution of this ADS command

BUSY

BOOL

Busy-Flag

ERR

BOOL

Error-Flag

ERRID

UDINT

ADS error code

Function block ADSWRITE in TwinCat

../../_images/Funktionsblock_ADSWRITE_DE.png

TwinCat – ADSWRITE

ADSWRITE commands

Name

Type

Inherited from

Address

Initial

Comment

NETID

T_AmsNetId

Ams net id

PORT

T_AmsPort

ADS communication port

IDXGRP

UDINT

Index group

IDXOFFS

UDINT

IndexOffset

LEN

UDINT

Maximum number of the data bytes to be written (LEN ≤ maximum size of source buffer)

SRCADDR

PVOID

Indicator of source buffer

WRITE

BOOL

Rising edge starts command execution.

TMOUT

TIME

DEFAULT_ADS_TIMEOUT

Maximum permissible time for the execution of this ADS command

BUSY

BOOL

Busy-Flag

ERR

BOOL

Error-Flag

ERRID

UDINT

ADS error code

Preparation for the web server

EoE set-up

In order to be able to access the web server of the BNI module, access via EoE (Ethernet over EtherCAT) must be configured first.

  1. Select the Advanced Settings… button.

    ../../_images/Schaltflaeche_Advanced_Settings.png

    Advanced Settings… button

  2. Enter valid DNS name and valid IP address.

    ../../_images/DNS-Name_gueltige_IP.png

    Enter valid DNS name and valid IP address

Preparing network

Before the web server can be reached via EoE, the network of the Beckhoff control must be configured.

Configuring Beckhoff control

A static IP address must be assigned to both network cards.

  1. On the Beckhoff control select Start > Control panel Network and dial-up connections > PCI…Settings.

  2. Assign IP address.

    ../../_images/IP-Adresse_vergeben.png

    Advanced Settings… button

  3. Under Start > Control Panel > Beckhoff CX Configuration Tool > Miscellaneous activate the setting IP Routing.

    ../../_images/IP_Routing_aktivieren.png

    Advanced Settings… button

EoE and PC networks

For the EoE settings in the Twincat, the IP address of the second network card of the Beckhoff control must be entered as a default gateway.

As a default gateway for the network configuration of the PC, the IP address of the first network card of the Beckhoff control must be entered.

Object directory

Map TxPDO input pin 2 (0x1A90)

Input Pin 2, one bit for each port.

Map TxPDO pin 4 (0x1A0n)

The following index range applies in a modular EtherCAT device:
  • 0x6xxx is a module-specific input range for TxPDO data.

  • 0x7xxx is a module-specific output range for RxPDO data.

IO-Link data is up to 32 bytes for input and output.

If a connection is configured as aDigital InputorDigital Output, the value of pin 4 is mapped to data byte 0, bit 0.

Map TxPDO PowerStatus (0x1A91)

Index

Subindex

Name

DataType

0xF601

0x01

Global status, see Global status values (Subindex 0x01)

UINT8

0x02

Short circuit in the sensor supply; one bit for each port

UINT8

0x03

Short circuit at pin 4 of the actuator supply, one bit for each port

UINT8

0x04

Short circuit at pin 2 of the actuator supply, one bit for each port

UINT8

Global status values (Subindex 0x01)

Bit

Description

0

Sensor supply low (1 = low, 0 = OK)

1

Actuator supply low (1 = low, 0 = OK)

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

Index

Sub-index

Name

DataType

Access

0x40n0

0x01

Control

UINT8

RW

0x02

Status

UINT8

RO

0x03

Index

UINT16

RW

0x04

Subindex

UINT8

RW

0x05

Length

UINT8

RW

0x06

Data

UINT32

RW

n = 0…7

0x07

Error code

UINT16

RO

Control values (Subindex 0x01)

Value (UINT8)

Function

0

no control action

2

write

3

read

Status values (Subindex 0x02)

Value (UINT8)

Status

0

no activity

1

busy

2

success

4

error

0xFF

failure

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

Index

Sub-index

Name

Value

DataType

0x8nn0
n = 0…7

0x04

Device ID

24-Bit-ID

UINT32

0x05

Vendor ID

16-Bit-ID

UINT32

0x32

IO-Link revision

0x10 or 0x11

UINT8

0x33

Frame Capability

not in use

UINT8

0x34

Desired Cycle Time

Cycle Time

UINT8

0x35

Offset Time

not in use

UINT8

0x36

Max. PD In Length

Max. length

UINT8

0x37

Max. PD Out Length

Max. length

UINT8

0x38

Compatible ID

not in use

UINT16

0x40

Master Control

see Configuration without ESI.

UINT16

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

Index

Subindex

Name

DataType

Access

0x90n0, n = 0…7

0x04

Device ID

UINT32

RO

0x05

Vendor ID

UINT32

RO

0x20

IO-Link revision

UINT8

RO

0x22

Min Cycle Time

UINT8

RO

0x24

Process Data In Length

UINT8

RO

0x25

Process Data Out Length

UINT8

RO

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

Index

Subindex

Name

DataType

Access

0xa0n0
n = 0…7

0x01

IO-Link state

UINT8

RO

0x02

Lost Frames

UINT8

RO

Value

Name

Status of IO-Link Port

0

INACTIVE

Deactivated

1

DIGINPUT

Digital Input

2

DIGOUTPUT

Digital Output

3

ESTABLISHCOMM

not in use

4

INITMASTER

not in use

5

INITDEVICE

not in use

6, 7

Unused

not in use

8

OPERATE

IO-Link, in status Operate

9

STOP

IO-Link, not in status Operate state (error or no device)

Values for Lost Frames (Subindex 0x02)

This parameter counts lost IO-Link Frames (M sequence repeats).

Two repeat attempts are generally added when changing the device. This value is only reset to zero during the start. The value is updated regularly, e.g. once a second.

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

Index

Subindex

Name

DataType

Access

0xF100

0x01

Status of IO-Link Port 1

UINT8

RO

0x02

Status of IO-Link Port 2

UINT8

RO

0x03

Status of IO-Link Port 3

UINT8

RO

0x04

Status of IO-Link Port 4

UINT8

RO

0x05

Status of IO-Link Port 5

UINT8

RO

0x06

Status of IO-Link Port 6

UINT8

RO

0x07

Status of IO-Link Port 7

UINT8

RO

0x08

Status of IO-Link Port 8

UINT8

RO

The CoE objectDevice Status(0xF100) is mapped asTxPDO-Mapping of Status Datato the Process Data.

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

Index

Subindex

Name

DataType

Access

0xF101

0x01

Port Qualifier Port 1

UINT8

RO

0x02

Port Qualifier Port 2

UINT8

RO

0x03

Port Qualifier Port 3

UINT8

RO

0x04

Port Qualifier Port 4

UINT8

RO

0x05

Port Qualifier Port 5

UINT8

RO

0x06

Port Qualifier Port 6

UINT8

RO

0x07

Port Qualifier Port 7

UINT8

RO

0x08

Port Qualifier Port 8

UINT8

RO

The CoE objectPort Qualifier(0xF101) is mapped asTxPDO-Mapping of Port Qualifierto the Process Data.

Port Qualifier Bits

Bit

Description

4

PortActive / Port activated
1 = Port can be used.
2 = Port deactivated.

5

DevCom / device is ready for operation
1 = Device detected and in status Operate
0 = everything else

6

DevErr / device error
1 = Error occurred (validation error, short circuit, etc.)
0 = OK

7

PQ / validity of input data of IO-Link device
1 = valid
0 = invalid

Configuration without ESI

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants

The ports can also be configured without integration of an ESI. For this, the master control and the respective length of the process data must be set in the object 0x8000.

Values for the master control (80X0:28)

Value

Function

0x0000

Deactivated

0x0001

Port in Standard Input

0x0002

Port in Standard Output

0x0003

Port in IO-Link mode

0x0005

Power

Process data length

IO-Link Ports

Byte

Length of data

1 Byte

0x08

2 Byte

0x16

4 Byte

0x83

6 Byte

0x85

8 Byte

0x87

10 Byte

0x89

16 Byte

0x8F

24 Byte

0x97

32 Byte

0x9F

Standard input/output ports

0x01

Example

MasterControl = 3 –> IO-Link

IO-Link size

Process Data In Length

Process Data Out Length

Hex

Dec

Hex

Dec

IOL_l_1byte

0x08

8

0x00

0

IOL_l_2byte

0x16

22

0x00

0

IOL_l_4byte

0x83

131

0x00

0

IOL_l_6byte

0x85

133

0x00

0

IOL_l_8byte

0x87

135

0x00

0

IOL_l_10byte

0x89

137

0x00

0

IOL_l_16byte

0x8F

143

0x00

0

IOL_l_24byte

0x97

151

0x00

0

IOL_l_32byte

0x9F

159

0x00

0

IOL_l_1byte/0_1bytes

0x08

8

0x08

8

IOL_l_2byte/0_2bytes

0x16

22

0x16

22

IOL_l_2byte/0_4bytes

0x16

22

0x83

131

IOL_l_4byte/0_4bytes

0x83

131

0x83

131

IOL_l_4byte/0_2bytes

0x83

131

0x16

22

IOL_l_2byte/0_8bytes

0x16

22

0x87

135

In the start-up the configuration for Port 6 in IO-Link mode with 32 Byte process data length for input and output looks as follows:

../../_images/Beispiel_Port_6.png

Sample configuration in the start-up for Port 6