Ethernet/IP integration
Integration in RSLogix EIP development tool
Example of how the module can be integrated into the RSLogix EIP development tool:
Go offline.
Right click on Ethernet (the correct scanner card) and select New Module….
Select the Generic Ethernet Module as Ethernet module in the communication path.
Enter tag name (user-defined), select the general format Data SINT, enter the IP address of the module and the correct connection parameters and confirm with OK.
⇒ The new module and the corresponding controller tags are automatically generated.
Download the configuration with Download.
After the download is completed the tags can be monitored and activated using the Controller tags option.
Note
Make sure to select the previously configured correct tag name.
The entry, output and configuration data are described on the following pages.
Note
These tags can also be used for programming.
Integration
Data configuration
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Enter the values from Data configuration in the control system. They describe the data sizes of the entry, output and configuration data.
Automatic IO-Link – Adjustable IO-Link process data length
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
The Ethernet/IP master offers a variety of configurations for IO-Link process data lengths, ranging from 0 to 32 bytes. The EDS file (Electronic Data Sheet) contains several predefined connections under the Connection Manager section. One of these connections is, for example, Connection2 with the name Exclusive Owner Connections – 32 IOL Data. A connection is a compilation of a configuration. Part of this is the definition of the data from the control unit to the device (O->T), the data from the device to the control unit (T->O) and the device configuration. These definitions can be found in the EDS file under the Assembly section. Assem101 (a consuming module with 32 bytes of IO-Link output process data) is used for Connection2 and the direction _O->T. Assem100 (a producing module with 32 bytes of IO-Link input process data) is used for the direction T->O and Assem102 is used for the configuration.
For example, if 10 bytes of IO-Link input and output data are required, the path 20 04 2C 73 2C 72 (hex) can be used, where the assembly sizes are T->O 216, O->T 86 and the configuration assembly is 0 or 58 bytes.
Configuration modules
The Ethernet/IP master contains two configuration assemblies for managing the IO-Link settings. These are Assem102 and Assem103, which each serve different purposes:
Assem102: The assignment of this module is described in detail in the EDS file and can be configured to a size of either 58 bytes or 0 bytes. If it is set to 0 bytes, the existing configuration is retained and is not overwritten.
Assem103: This module is set to a length of 0 bytes and was specially developed to automatically set all ports to IO-Link mode.
If the configuration module is not included in the connection path, the device operates as if module 103 is being used. This means that all ports are automatically set to IO-Link mode.
Configuration data
Assignment of configuration data sequence shows an assignment of the configuration data sequence. The stated standard values describe a configuration with the IO-Link function on Pin 4 and standard I/O functions on Pin 2 and 4 of every port. The input and output functions of the configured standard I/O ports are set using the process data.
Module configuration
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
IO-Link Port configuration
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Byte |
Description |
|---|---|
2 |
Port X01 Cycle time |
3 |
Port X01 Validation type and parameter server |
4, 5 |
Port X01 Vendor ID |
6…8 |
Port X01 Device ID |
… |
Cycle settings
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
With this parameter, the IO-Link communication speed can be set. The IO-Link cycle time can be increased calculated by the multiplier and the time base.
The time base is described in the table below, the multiplier is entered as a decimal number from 0…63.
The cycle-time byte is structured as follows:
Bits 0…5 (Multiplier): These bits contain a 6-bit multiplier for calculating MasterCycleTime or MinCycleTime. The valid range is 0…63.
Bits 6…7 (Time base): These bits define the time base used to calculate MasterCycleTime or MinCycleTime.
Bit position |
Description |
|---|---|
7 |
Time base bit 1 |
6 |
Time base bit 0 |
5 |
Multiplier bit 5 |
4 |
Multiplier bit 4 |
3 |
Multiplier bit 3 |
2 |
Multiplier bit 2 |
1 |
Multiplier bit 1 |
0 |
Multiplier bit 0 |
Possible values for MasterCycleTime and MinCycleTime:
Time base coding |
Time base value |
Calculation |
Cycle Time |
|---|---|---|---|
00 |
0.1 ms |
Multiplier x time base |
0.41[1] …6.3 ms |
01 |
0.4 ms [1] |
6.4 ms + multiplier x time base |
6.4…31.6 ms |
10 |
1.6 ms |
32 ms + multiplier x time base |
32…132.8 ms |
11 |
reserved |
reserved |
reserved |
Validation settings
No validation : Validation deactivated, every device is accepted.
Compatibility : Manufacturer ID and Device ID are compared with the data of the IO-Link device.
Parameter server
Switched on : Data retention functions active, parameter data and identification data of the IO-Link device are saved in a remanent memory.
Switched off : Data retention functions deactivated, saved parameter data and identification data of the IO-Link devices remain in the memory.
Enable download : If only the download is enabled, in each case the master starts a download of the parameter data. In this case the download is also performed irrespective of the upload flag of the IO-Link device. If there are no data in the master port, an upload takes place first (e.g. after deletion of the data or before the first data upload). Upload and download enabled: If the upload and download are enabled, a distinction is made for different parameter records depending on the upload flag of the IO-Link device. If there are no data in the IO-Link master port, an initial upload takes place (e.g. after deletion of the data or before the first data upload). If the upload flag is set at the IO-Link device, the parameter data are uploaded in each case. If no upload flag is set and parameter data have already been stored, a download of the parameter data takes place in each case.
Note
After uploading the parameter data, the Vendor ID and Device ID of the connected IO-Link device remain stored until the data records are deleted.
When the connected IO-Link device is started a validation takes place and then only an IO-Link device of the same type can be used for the data retention.
If a different type of IO-Link device should be used, the content of the parameter server must be deleted.
The data storage is only supported by IO-Link devices with IO-Link Revision 1.1.
Values for validation type and parameter server
Upload flag at IO-Link device
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
The upload flag is required in order to overwrite data already saved in the parameter server with new parameter data of the same IO-Link device.
In order to activate the upload flag of an IO-Link device, the data value 0x05 must be entered in the index 0x02, subindex 0.
(For information on setting parameters via IO-Link, see I/O ports or IO-Link device parameterization.
Configuration via Explicit Messages
PLC program
Note
Information about the PLC program and Add Application Logic , see Allen Bradley Ethernet/IP QuickConnect Application Technique.
Fault State
For each output at the port pins, a safe state can be predefined, which should be adopted in the case of a loss of bus communication.
The Fault State settings can be implemented via the following Class Instance Attribute of the Explicit Messages.
Activate / deactivate Fault State
Class |
Instance |
Attribute |
Value |
|---|---|---|---|
9 (0x09) |
1 – m [2] |
6 |
|
Fault State Action
Class |
Instance |
Attribute |
Value |
|---|---|---|---|
9 (0x09) |
1 – m [2] |
5 |
|
Note
The Fault State settings are only stored temporarily in the module. They are deleted again after a power reset.
In order to ensure a permanent Fault State configuration, the configuration must be programmed via the PLC so that it can be transferred to the module again when the system is restarted.
IO-Link device parameterization
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
There are two ways to parameterize an IO-Link device connected to the IO-Link Port.
Parameterization via the web server (see I/O ports)
Parameterization via Explicit Messages
The following section describes, for example, how via Rockwell RSLogix 5000 an IO-Link device can be parameterized via Explicit Messages.
The MSG modules are used in the PLC program (see MSG modules).
Read IO-Link parameters
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Service code |
Class |
Instance |
Attribute |
|---|---|---|---|
0x32 |
0x96 |
1…n [3] |
0x03 (Read parameters) |
Source Length must at least correspond to the read parameters, but can also be bigger (in this example 100 bytes).
As a Source Element (Write) and as a Destination Element (Read), create a SINT[100] Array and select the first row [0].
In the Source Element Array (Write) enter which index should be read (in this example Index 0x4E).
⇒ The read value is displayed in the Destination Element Array (Read).
⇒ The error code is also displayed there in the event of a parameterization error.In the Communication window select the Ethernet module for which parameters should be set.
Write IO-Link parameters
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Service code |
Class |
Instance |
Attribute |
|---|---|---|---|
0x32 |
0x96 |
1 - n [3] |
0x02 (Write parameters) |
Select Source Element and Destination Element as described in the example Values for read IO-Link parameters.
The Source Length must be the same length as the parameter data to be written. In this example the index 0x4E, subindex 0, value 0x02 are written in the Source Element Array (Write).
In the event of a parameterization error an error code is displayed in the Destination Element Array (Read).
In the Communication tab select the Ethernet module for which parameters should be set.
Note
The Explicit Messages functions are implemented according to Volume 1: Common Industrial Protocol Specification and Volume 2: Ethernet/IP Adaption of CIP.
Process data
Process data inputs
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
The input data have a size of 392 bytes. The table below shows the assignment of the process data inputs.
Standard input data
| Byte | Bit | Description | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | ||
| 0 | I32 | I34 | I22 | I24 | I12 | I14 | I02 | I04 |
Input data I04: Input for Port 0, Pin 4 The result is only 0 when the port is configured as an IO-Link Port. |
| 1 | I72 | I74 | I62 | I64 | I52 | I54 | I42 | I44 | |
| 2 | S3 | S2 | S1 | S0 |
Short circuit status Short circuit between Pin 1 and 3 at reported port |
||||
| 3 | S7 | S6 | S5 | S4 | |||||
| 4 | O32 | O34 | O22 | O24 | O12 | O14 | O02 | O04 |
Overload status O04: Overload at Port 0, Pin 4 Only if the port is configured as an output. [4] |
| 5 | O72 | O74 | O62 | O64 | O52 | O54 | O42 | O44 | |
| 6 | 0 | 0 | 0 | 0 | 0 | NA | PS |
PA [4] |
Status of power supply NA: No actuator supply PS: Power supply of sensor PA: Power supply of actuator |
| 7 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | reserved |
IO-Link input data
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
| Byte | Bit | Description | ||||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |||
| 8…39 | IO-Link Port 0 input data | |||||||||
| 40 | 0 | 0 | 0 | 0 | 0 | 0 | DC | IOL |
IO-Link status IOL: Port in IO-Link mode DC: Device connected 0: reserved |
|
| 41 | SC | 0 | 0 | 0 | 0 | PDI | DF | VF |
IO-Link error VF: Validation failed SC: IO-Link short-circuit DF: Data storage validation failed PDI: Process data invalid |
|
| 42 | Manufacturer code 1 | Manufacturer code | ||||||||
| 43 | Manufacturer code 2 | |||||||||
| 44 | Device code 1 | Device code | ||||||||
| 45 | Device code 2 | |||||||||
| 46 | Device code 3 | |||||||||
| 47 | Mode | Type | 0 | Event 1 | Mode: 0: reserved 1: Single event 2: Event outgoing 3: Event incoming Type: 0: reserved 1: Message 2: Warning 3: Error | |||||
| 48 | Event code high | |||||||||
| 49 | Event code low | |||||||||
| 50 | Mode | Type | 0 | Event 2 | ||||||
| 51 | Event code high | |||||||||
| 52 | Event code low | |||||||||
| 53 | Mode | Type | 0 | Event 3 | ||||||
| 54 | Event code high | |||||||||
| 55 | Event code low | |||||||||
| … | The data of the other IO-Link Ports are structured identically and described below. | |||||||||
Process data outputs
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
The output data have a size of 262 bytes. The table below shows the assignment of the process data outputs.
Byte |
Module part |
Description |
|---|---|---|
0…5 |
Standard I/O ports |
Process data outputs for the standard inputs |
6…37 |
IO-Link Port 0 |
Process data output for the IO-Link Port 0 |
38…69 |
IO-Link Port 1 |
Process data output for the IO-Link Port 1 |
70…101 |
IO-Link Port 2 |
Process data output for the IO-Link Port 2 |
102…133 |
IO-Link Port 3 |
Process data output for the IO-Link Port 3 |
134…165 |
IO-Link Port 4 |
Process data output for the IO-Link Port 4 |
166…197 |
IO-Link Port 5 |
Process data output for the IO-Link Port 5 |
198…229 |
IO-Link Port 6 |
Process data output for the IO-Link Port 6 |
230…261 |
IO-Link Port 7 |
Process data output for the IO-Link Port 7 |
Standard output data
Byte |
Bit |
Description |
|||||||
|---|---|---|---|---|---|---|---|---|---|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
||
0 |
O32 |
O34 |
O22 |
O24 |
O12 |
O14 |
O02 |
O04 |
Output data O04: Output at Port 0, Pin 4 The port must be configured as |
1 |
O72 |
O74 |
O62 |
O64 |
O52 |
O54 |
O42 |
O44 |
see above |
2 |
R32 |
R34 |
R22 |
R24 |
R12 |
R14 |
R02 |
R04 |
Restart Restart of output after identified short-circuit |
3 |
R72 |
R74 |
R62 |
R64 |
R52 |
R54 |
R42 |
R44 |
see above |
4 |
0 |
0 |
0 |
0 |
0 |
0 |
0 |
0 |
reserved |
5 |
0 |
0 |
0 |
0 |
0 |
DL |
GO |
RO |
Display control [6] |
IO-Link output data
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Byte |
Bit |
Description |
|||||||
|---|---|---|---|---|---|---|---|---|---|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
||
6…37 |
IO-Link Port 0 output data |
||||||||
… |
The data of the other IO-Link Ports are structured identically and |
Quick Connect mode
The following points must be observed in Quick Connect operating mode:
Ethernet port settings
Ethernet port 1: The connection must be set to a fixed speed of 100 Mbit/s in full duplex mode.
Ethernet port 2: The connection must be set to a fixed speed of 100 Mbit/s in full duplex mode.
Device configuration: Quick Connect mode must be activated.
Auto-MDIX is not available in Quick Connect mode. Therefore, the automatic configuration of the ports at fixed speed and activated Quick Connect is as follows:
Port 1: MDI
Port 2: MDIX
This configuration is crucial, as port 2 can be connected to port 1 of another device with a non-crossover cable, but not to port 2. If the connection is incorrect, no Ethernet connection (link) can be established.
For more information, see Ethernet/IP Specification Volume 2: EtherNet/IP Adaption of CIP, Appendix E: EtherNet/IP Quick Connect™.