Modbus TCP configuration
Description
Modbus is available in masters as an interface with the following features:
Read/write process data
Port configuration
Port/device diagnostics
Read/write ISDU data
Access is via the TCP/IP interface using the IP address of the device and Port 502 (example: 192.168.1.1:502). The response time depends on the data written/read.
Structure of a Modbus TCP message
A Modbus TCP message is structured as follows:
Byte 0 |
Byte 1 |
Byte 2 |
Byte 3 |
Byte 4 |
Byte 5 |
Byte 6 |
Byte x |
|---|---|---|---|---|---|---|---|
Transaction ID |
Protocol ID |
Unit ID |
Function Code |
Data |
|||
MBAP header |
PDU |
||||||
Modbus TCP message |
|||||||
The protocol ID must be 0, as it indicates that the message is a Modbus message.
The unit ID can be arbitrary. It is not used because the IP address already identifies a device.
General
All numbers are decimal numbers, unless they are specified with 0x = hexadecimal, e.g.: 0x1B.
All data is organized as UINT16 unless otherwise specified.
The length is organized in UINT16 by default, unless otherwise specified, e.g. length in [bytes] or bit length.
The mapping of the byte sequence uses Big Endianness, see example in Index 10.
The Profile ID
Note
The Register Mapping Version (list of registers and their content) is identified with the Profile ID which is a similar version number to HW or FW version number. Due to the content of the registers may be subject to change in the future, with keeping the compatibility and consistency, this Profile ID should be checked first when a new application is developed.
Index overview
Profile ID = 2
Available from Firmware 1.3.1
Index (dec.) |
Description |
Access |
|---|---|---|
|
Profile ID (Register Mapping Version) |
RO |
|
Device (Module) Identification |
RO |
|
IO-Link ISDU Command Request |
RW |
|
IO-Link ISDU Command Response |
RO |
|
IO-Link Process Data Input/Output |
RO/RW |
|
SIO Digital Input State |
RO |
|
SIO Digital Output State |
RW |
|
Digital Input State (Mirrored to 2000) |
RO |
|
Digital Output State (Mirrored to 2001) |
RW |
|
Device (Module&Port) Diagnostic |
RO |
|
IO-Link Port Diagnostic |
RO |
|
Port Configuration |
RW |
|
Variable Processdata Register |
RW |
|
Module Settings |
RW |
Identification
Index |
Length |
Description |
Access |
Default (example) |
|---|---|---|---|---|
0 |
1 |
Register Mapping Version (ProfileID) |
RO |
0x0001 |
1…9 |
- |
reserved |
- |
- |
10…13 |
4 |
Product Order Code (ASCII, 7 chars) |
RO |
BNI00KH |
14…29 |
16 |
Product Name (TEXT) |
RO |
BNI XG5-508-0B5-R067 |
30…99 |
- |
reserved |
- |
- |
The byte array from/to IO-Link is converted as follows in the MODBUS index:
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
UINT16 |
LSB |
Bit(0…7) |
= IO-Link Byte[n] |
|---|---|---|---|
UINT16 |
MSB |
Bit(8…15) |
= IO-Link Byte[n+1] |
Example
The ASCII coded text of the manufacturer nameBalluff(length = 7) is converted into four (4) Word UINT16 indices as follows:
Index |
0 |
1 |
2 |
3 |
4 |
5 |
6 |
|---|---|---|---|---|---|---|---|
Byte [0…6] |
42h, |
41h, |
4Ch, |
4Ch, |
55h, |
46h, |
46h |
Word[0…3] |
4142h, |
4C4Ch, |
4655h, |
0046h |
|---|---|---|---|---|
Index |
0 |
1 |
2 |
3 |
Read ISDU data
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Write the port number, index and subindex to the corresponding registers (30,31,32).
Write the selected command to the upper byte of register 33.
Write ISDU data
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Write the port number, index and subindex to the corresponding registers (30,31,32).
Write data to registers 35…51 and the desired data length.
Write the selected command to the upper byte of register 33.
Function Codes
The following function codes are implemented:
Read holding register (0x03)
Write several registers (0x10)
Error Responses
The following responses are reported in the event of an error:
Error Code |
Description |
|---|---|
0x00 |
No error. Last command successful. |
0x01 |
Bad Function Code |
0x02 |
Wrong Register Address |
0x03 |
Invalid value |
0x04 |
Slave error (IO-Link fails) |
Even if the start register is valid, reading too many registers leads to Bad Register Address.
Slave errors occur when the IO-Link interface triggers errors.
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Modbus TCP configurations
Digital Input / Output State
When a port (X01…X08) is configured as SIO mode (Standard Input or Output) following Digital Input / Output State can be accessed.
Registers 2000, 2001 and 2047, 2048 – Digital Input / Output State
There are two register locations which can be used for Digital Input and Output. Those are working completly the same and are just mirrored location for compatibility.
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
2000 (2047) |
- |
0…7 |
Digital Input Port n Pin 4 |
BOOL |
RO |
0 = off, 1 = on |
8…13 |
Digital Input Port n Pin 2 |
BOOL |
RO |
0 = off, 1 = on |
||
2001 (2048) |
- |
0…7 |
Digital Output Port n Pin 4 |
BOOL |
R/W |
0 = off, 1 = on |
8…13 |
Digital Output Port n Pin 2 |
BOOL |
R/W |
0 = off, 1 = on |
The digital output works if the port is configured as an output.
Values – Digital Input / Output State (data)
Value |
Description |
|---|---|
0 |
off, de-energized, 0 V |
1 |
on, under power, 24 V |
Bits – Digital Input / Output State (data)
Bit |
Port n |
|---|---|
0, 8 |
X01 |
1, 9 |
X02 |
2, 10 |
X03 |
3, 11 |
X04 |
4, 12 |
X05 |
5, 13 |
X06 |
6, 14 |
X07 |
7, 15 |
X08 |
Detailed view – Digital Input / Output State (data)
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
2000 (2047) |
0 |
0 |
X01 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
1 |
X02 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
2 |
X03 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
3 |
X04 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
4 |
X05 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
5 |
X06 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
6 |
X07 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
7 |
X08 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
1 |
0 |
X01 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
|
1 |
X02 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
2 |
X03 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
3 |
X04 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
4 |
X05 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
5 |
X06 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
6 |
X07 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
7 |
X08 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
2001 (2048) |
0 |
0 |
X01 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
1 |
X02 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
2 |
X03 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
3 |
X04 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
4 |
X05 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
5 |
X06 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
6 |
X07 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
7 |
X08 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
1 |
0 |
X01 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
|
1 |
X02 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
2 |
X03 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
3 |
X04 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
4 |
X05 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
5 |
X06 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
6 |
X07 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
7 |
X08 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
IO-Link Process Data
When a port (X01…X08) is configured as IO-Link mode following Process Data Input and Output can be accessed.
There are two ways of handling the Process Data
Using fixed length 32 Bytes, accessing port-by-port allows simple, port organized access, however it requires multiple commands to perform
Using customizable variable lenght provides accessing content in one step, but pre-configuration is required
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Registers 1100…1800 - IO-Link Process Data (fixed length)
Read out an IO-Link port once.
Reading back the process data output is used for feedback (control).
Index |
Length |
Description |
Access |
|---|---|---|---|
1100 |
34 |
Port X01 IO-Link Process Data Input/Output |
RO |
1200 |
34 |
Port X02 IO-Link Process Data Input/Output |
RO |
1300 |
34 |
Port X03 IO-Link Process Data Input/Output |
RO |
1400 |
34 |
Port X04 IO-Link Process Data Input/Output |
RO |
1500 |
34 |
Port X05 IO-Link Process Data Input/Output |
RO |
1600 |
34 |
Port X06 IO-Link Process Data Input/Output |
RO |
1700 |
34 |
Port X07 IO-Link Process Data Input/Output |
RO |
1800 |
34 |
Port X08 IO-Link Process Data Input/Output |
RO |
Details – IO-Link Process Data 1100…1800
Index |
Length |
Description |
Access |
Value |
|---|---|---|---|---|
1n01 [5] |
1 |
Port n IO-Link Process Data Input Valid |
RO |
0 = invalid, 1 = valid |
1n01…1n16 [5] |
16 |
Port n IO-Link Process Data Input (Byte 1…32) |
RO |
– |
1n17 [5] |
1 |
Port n IO-Link Process Data Output Valid |
RW |
0 = invalid, 1 = valid |
1n18…1n33 [5] |
16 |
Port n IO-Link Process Data Output (Byte 1…32) |
RW |
– |
Port numbers – IO-Link Process Data 1100…1800
n [5] |
Port |
|---|---|
1 |
X01 |
2 |
X02 |
3 |
X03 |
4 |
X04 |
5 |
X05 |
6 |
X06 |
7 |
X07 |
8 |
X08 |
Registers 11000…11257 - Variable Processdata Registers
The registers mirror the registers 1100…1800. While the standard processdata registers are always 32-Bytes long for input and output processdata the variable processdata register adapt to the configured length.
Index |
Byte |
Name |
DataType |
Access |
Value / Description |
Note |
|---|---|---|---|---|---|---|
11000 |
0 |
IO-Link Process Data Input Valid |
UINT16 |
RO |
Each bit represents a port (Bit 0 → Port 1, etc.) |
|
1 |
Reserved |
UINT16 |
RO |
Always zero |
||
11001 |
0 |
IO-Link Process Data Output Valid |
UINT16 |
RW |
Each bit represents a port (Bit 0 → Port 1, etc.) |
|
1 |
Reserved |
UINT16 |
RW |
Write zero |
||
11002…11257 |
Variable Processdata Input/Output |
RW |
See port configuration for size and layout |
See blow for Layout |
The variable processdata registers mirror the standard processdata registers (1100…1800), but adapt to the configured input/output length per port.
Input and output data lengths are defined by the port configuration.
Reserved bytes must be zero when written and will always read as zero.
If a port is not configured to IO-Link the complete processdata will be omitted in this registers (see example).
Variable Processdata Layout
The variable processdata registers are organized as follows:
Input Processdata for Ports 1–8 (read-only)
Output Processdata for Ports 1–8 (read/write)
If the configured processdata length for a port does not align to a full word (2 bytes), a padding byte is added to ensure the next port’s processdata starts at the correct word boundary.
Note:
The Input Processdata section is read-only. Any write attempt will result in an error.
Section |
Port Number |
Access |
|---|---|---|
Input Processdata |
1 |
Read-only |
Input Processdata |
2 |
Read-only |
Input Processdata |
3 |
Read-only |
Input Processdata |
4 |
Read-only |
Input Processdata |
5 |
Read-only |
Input Processdata |
6 |
Read-only |
Input Processdata |
7 |
Read-only |
Input Processdata |
8 |
Read-only |
Output Processdata |
1 |
Read/Write |
Output Processdata |
2 |
Read/Write |
Output Processdata |
3 |
Read/Write |
Output Processdata |
4 |
Read/Write |
Output Processdata |
5 |
Read/Write |
Output Processdata |
6 |
Read/Write |
Output Processdata |
7 |
Read/Write |
Output Processdata |
8 |
Read/Write |
Example
Suppose the following configuration:
Port 1 Input: 3 bytes
Port 3 Input: 2 bytes
Port 4 Input: 5 bytes
Port 1 Output: 4 bytes
Port 3 Output: 1 byte
The layout will be:
Address |
Section |
Port |
Data Length |
Padding |
Word Boundary |
|---|---|---|---|---|---|
11002 + 0 |
Input Processdata |
1 |
3 bytes |
1 byte |
2 words |
11002 + 2 |
Input Processdata |
3 |
2 bytes |
0 |
1 word |
11002 + 3 |
Input Processdata |
4 |
5 bytes |
1 byte |
3 words |
11002 + 6 |
Output Processdata |
1 |
4 bytes |
0 |
2 words |
11002 + 8 |
Output Processdata |
3 |
1 byte |
1 byte |
1 word |
This ensures each port’s processdata starts at a word boundary, with padding bytes added as needed. Ports which have zero length configured or are not in IO-Link mode will not reserve space in the register.
IO-Link ISDU Data
Registers 100, 300 – Acyclic Command Channel (including ISDU Read/Write Request)
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Index |
Length |
Description |
Access |
Default |
|---|---|---|---|---|
100 |
4…121 |
IO-Link ISDU Command Request |
RW |
- |
300 |
5…122 |
IO-Link ISDU Command Response |
RO |
- |
Details – Registers 100…220 Command Request Channel = ISDU Read/Write Request
Index |
Byte |
Name |
Data Type |
Access |
Needed? |
Value |
|---|---|---|---|---|---|---|
100 |
- |
Command |
UINT16 |
RW |
M [1] |
1 = read, 2 = write |
101 |
- |
Port No. |
UINT16 |
RW |
M [1] |
1…8 |
102 |
- |
Index |
UINT16 |
RW |
M [1] |
0…0xFFFF |
103 |
- |
Subindex |
UINT16 |
RW |
M [1] |
0…255 |
104 [3] |
- |
Data Length [Byte] |
UINT16 |
RW |
O [2] |
1…232 |
105…220 [4] |
0 |
Data Byte n |
UINT8 |
RW |
O [2] |
- |
105…220 [4] |
1 |
Data byte n1 |
UINT8 |
RW |
O [2] |
- |
Details - Registers 300…421 Command Response Channel = ISDU Read/Write Response
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
300 |
- |
- |
Command (last sent) |
UINT16 |
RO |
1 = read, 2 = write |
301 |
- |
- |
Port No. |
UINT16 |
RO |
1…8 |
302 |
- |
- |
Index |
UINT16 |
RO |
0…0xFFFF |
303 |
- |
- |
Subindex |
UINT16 |
RO |
0…255 |
304 |
- |
- |
Error Code |
UINT16 |
RO |
0 = no error other values = see Tab. 6-15 |
305 |
- |
Data Length [Bytes] |
UINT16 |
RO |
1…232 |
|
306…421 |
0 |
- |
Data Byte n |
UINT8 |
RO |
- |
306…421 |
1 |
- |
Data Byte n+1 |
UINT8 |
RO |
- |
Error codes
Error Code |
Description |
|---|---|
0x0000 |
No error, command was successful |
0x4001 |
ARGBLOCK_NOT_SUPPORTED |
0x4002 |
ARGBLOCK_INCONSISTENT |
0x4003 |
DEVICE_NOT_SUPPORTED |
0x4004 |
SERVICE_NOT_AVAILABLE |
0x4005 |
DEVICE_NOT_IN_OPERATE |
0x4006 |
MEMORY_OVERRUN |
0x4011 |
PORT_NUM_INVALID |
0x4034 |
ARGBLOCK_LENGTH_INVALID |
0x4036 |
SERVICE_TEMP_UNAVAILABLE |
0x8000…0x80FF |
IO-Link error code from the connected device, see IO-Link specification |
Diagnostic
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Index |
Length |
Description |
Access |
|---|---|---|---|
3000 |
10 |
Module and Port Diagnostic |
RO |
3100 |
10 |
X01 IO-Link Info & Events |
RO |
3200 |
10 |
X02 IO-Link Info & Events |
RO |
3300 |
10 |
X03 IO-Link Info & Events |
RO |
3400 |
10 |
X04 IO-Link Info & Events |
RO |
3500 |
10 |
X05 IO-Link Info & Events |
RO |
3600 |
10 |
X06 IO-Link Info & Events |
RO |
3700 |
10 |
X07 IO-Link Info & Events |
RO |
3800 |
10 |
X08 IO-Link Info & Events |
RO |
Details – Diagnostic
Registers 3000…3009 – Module and Port Diagnostic
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
3000 |
0 |
0…3 |
reserved |
– |
RO |
– |
3000 |
0 |
4 |
Sensor Voltage Short Circuit |
BOOL |
RO |
– |
3000 |
0 |
5 |
Actuator Short Circuit |
BOOL |
RO |
– |
3000 |
0 |
6 |
Actuator Warning |
BOOL |
RO |
– |
3000 |
0 |
7 |
IO-Link Short Circuit |
BOOL |
RO |
– |
3001 |
0 |
0…7 |
Port n: IO-Link Communication Established |
BOOL |
RO |
– |
3001 |
1 |
8…15 |
Port n: IO-Link PD Input Valid |
BOOL |
RO |
– |
3002 |
0 |
0…7 |
Port n: IO-Link Valid Device Connected |
– |
– |
– |
3002 |
1 |
8…15 |
reserved |
– |
– |
– |
3003 |
– |
– |
reserved |
– |
– |
– |
3004 |
0 |
0…7 |
Port n: Actuator shutdown (Pin 2) |
BOOL |
RO |
– |
3004 |
1 |
8…15 |
Port n: Actuator shutdown (Pin 4) |
BOOL |
R |
– |
3005 |
0 |
0…7 |
Port n: Actuator Warning (Pin 2) |
BOOL |
RO |
– |
3005 |
1 |
8…15 |
Port n: Actuator Warning (Pin 4) |
BOOL |
RO |
– |
3006 |
– |
– |
reserved |
– |
– |
– |
3007 |
– |
– |
reserved |
– |
– |
– |
3008 |
– |
– |
reserved |
– |
– |
– |
3009 |
– |
– |
reserved |
– |
– |
– |
BOOL value |
Meaning |
|---|---|
0 |
false, status not available |
1 |
true, status available |
Bit |
Port n |
|---|---|
0, 8 |
X01 |
1, 9 |
X02 |
2, 10 |
X03 |
3, 11 |
X04 |
4, 12 |
X05 |
5, 13 |
X06 |
6, 14 |
X07 |
7, 15 |
X08 |
Registers 3010…3080 – IO-Link Port Diagnostic
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Detailed information about the connected IO-Link device.
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
3n00 [6] |
0 |
0 |
IO-Link Mode |
BOOL |
RO |
– |
1 |
Device Connected |
BOOL |
RO |
– |
||
2 |
Valid PD IN Data |
BOOL |
RO |
– |
||
3 |
Wrong Vendor ID or Device ID |
BOOL |
RO |
– |
||
4 |
Wrong Cycle Time |
BOOL |
RO |
– |
||
5 |
Wrong Length PD IN |
BOOL |
RO |
– |
||
6 |
Wrong Length PD OUT |
BOOL |
RO |
– |
||
7 |
reserved |
– |
RO |
– |
||
1 |
– |
reserved |
– |
RO |
– |
|
3n01 [6] |
– |
– |
Vendor ID |
UINT16 |
RO |
– |
3n02 [6] |
0 |
– |
Device ID (MSB) |
UINT8 |
RO |
– |
1 |
– |
reserved |
– |
RO |
– |
|
3n03 [6] |
– |
– |
Device ID (LSB) |
UINT16 |
RO |
– |
3n04 [6] |
0 |
– |
Entry #1 Event Qualifier |
IOL coded |
RO |
IOL coded |
1 |
– |
reserved |
– |
RO |
– |
|
3n05 [6] |
– |
– |
Entry #1 Event Code |
UINT16 |
RO |
IOL coded |
3n06 [6] |
0 |
– |
Entry #2 Event Qualifier |
Enum |
RO |
IOL coded |
1 |
– |
reserved |
– |
RO |
– |
|
3n07 [6] |
– |
– |
Entry #2 Event Code |
UINT16 |
RO |
IOL coded |
3n08 [6] |
0 |
– |
Entry #3 Event Qualifier |
Enum |
RO |
IOL coded |
1 |
– |
reserved |
– |
RO |
– |
|
3n09 [6] |
– |
– |
Entry #3 Event Code |
UINT16 |
RO |
IOL coded |
Port numbers – Registers 3010…3080
n [5] |
Port |
|---|---|
1 |
X01 |
2 |
X02 |
3 |
X03 |
4 |
X04 |
5 |
X05 |
6 |
X06 |
7 |
X07 |
8 |
X08 |
IOL coded Event Qualifier – Registers 3010…3080
Bit |
Description |
|---|---|
0…2 |
Instance |
3 |
Source |
4…5 |
Type |
6, 7 |
Mode |
Configuration
Registers 9100…9800 – Port Configuration
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Index |
Length |
Name |
|---|---|---|
9100 |
7 |
X01 Port Configuration |
9200 |
7 |
X02 Port Configuration |
9300 |
7 |
X03 Port Configuration |
9400 |
7 |
X04 Port Configuration |
9500 |
7 |
X05 Port Configuration |
9600 |
7 |
X06 Port Configuration |
9700 |
7 |
X07 Port Configuration |
9800 |
7 |
X08 Port Configuration |
Please see the following tables for information on the structure of the port configuration.
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
9n00 [5] |
0 |
- |
Master Cycle Time |
UINT8 |
RW |
IO-Link coded |
1 |
- |
reserved |
- |
- |
||
9n01 [5] |
0 |
- |
Pin 2 Port Mode |
UINT8 |
RW |
0 = deactivated 1 = Digital Input 2 = Digital Output |
1 |
- |
Pin 4 Port Mode |
UINT8 |
RW |
0 = deactivated 1 = IOL Manual 2 = IOL Autostart 3 = Digital input |
|
9n02 [5] |
0 |
- |
Validation ID |
UINT8 |
RW |
0 = No device check 1 = Compatible V1.0 2 = Compatible V1.1 3 = Backup |
1 |
- |
reserved |
- |
- |
- |
|
9n03 [5] |
- |
- |
Vendor ID |
UINT16 |
RW |
- |
9n04 [5] |
0 |
- |
Device ID (MSB) |
UINT8 |
RW |
- |
1 |
- |
reserved |
- |
- |
- |
|
9n05 [5] |
- |
- |
Device ID (LSB) |
UINT16 |
RW |
- |
Port numbers – Registers 9100…9800
n [5] |
Port |
|---|---|
1 |
X01 |
2 |
X02 |
3 |
X03 |
4 |
X04 |
5 |
X05 |
6 |
X06 |
7 |
X07 |
8 |
X08 |
Coding of the master cycle time of the IO-Link specification
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants
Time Base Encoding |
Time Base Value |
Calculation |
Cycle Time |
|---|---|---|---|
0 |
0.1 ms |
Multiplier × Time base |
0.4…6.3 ms |
1 |
0.4 ms |
6.4 ms + Multiplier × Time Base |
6.4…31.6 ms |
10 |
1.6 ms |
32.0 ms + Multiplier × Time Base |
32.0…132.8 ms |
11 |
reserved |
reserved |
reserved |
Register 20000 - Module Settings
Global configuration registers for the Module (Device).
Index |
Byte |
Bit |
Name |
DataType |
Access |
Value |
Note |
|---|---|---|---|---|---|---|---|
20000 |
Output Powerloss Behavior |
UINT16 |
RW |
See table below |
(1) |
(1) Only available for the XG5-538 Variants
Value |
Description |
|---|---|
0 |
Default. The Network Module will imitate the behavior of a XGx-508 master. |
If UA is lost/ not connected also the US powered outputs will be deactivated by software |
|
1 |
No Software Handling enabled. Powerloss behavior is defined by the hardware. |