Extension by IO-Link master¶
You can expand the CMTK with additional IO-Link connections by connecting an Ethernet/IP-based IO-Link master.
Supported IO-Link masters¶
The following IO-Link masters are supported:
- BNI006A (BNI EIP-508-105-Z015)
- BNI009T (BNI EIP-507-005-Z040)
- BNI00H7 (BNI EIP-508-105-Z067)
- BNI00HM (BNI EIP-508-005-Z015-013)
Integrate IO-Link master¶
-
Connect the IO-Link master directly to the CMTK via LAN port 1 or LAN port 2 and ensure that the IO-Link master is accessible to the CMTK within the LAN.
Note
IO-Link masters often have a static IP preset at the factory. For connection to LAN port 1 or LAN port 2, this must be adapted, e.g. to Manual within the same IP range.
-
Navigate to the Connected Devices menu and click * Add Master*.

A search is made for reachable IO-Link masters.
Note
Please make sure that the network ports within your network are enabled.

-
Click CONNECT to connect the CMTK to the IO-Link master.The IO-Link master appears under the CMTK.

You can make all other settings as usual for the sensors connected to the IO-Link master.