Alerts are based on Grafana. Here only the configuration of the Alerts is explanined. You can find detailed informations about Grafana in the Visualization manual.
"Evaluation": In this time interval, the condition is checked.
Example: Every 30 seconds, the condition is checked.
"Time Range": In this range, it's checked, if the condition is true.
Example: The avarage value of the last 30 seconds is checked.
"Pending": If you don't like to raise an alarm immediately, you can use it. It keeps the alarm in a pending state for a defined time before raising the alert.
Example: After 60 seconds, the alarm raised. Before, its in pending state.
"When": Here you can select the type of the condition.
Example: average, minimal or maximum value.
"Of": Here you can select the measurement value of the sensor, which is used for the alert.
Example: vibration or contact temperature.
"Is above": You can change it to another type of comparison and set the comparison value.
Example: you can select "is above", "is below" or others and enter a value. Alert settings
Save alert
After setting the conditions, click on "Save Alert".
Alert settings example
After saving, this notification on the top right of the screen will pop up.
Success popup
Alert shows up
When the alert conditions are true, a pending and alerting line will show up. You may need to refresh the graph to see it.
Pending and alert in graph
In this case it gets triggered immediately, because the temperature is above 25° all the time. Alert ongoing
The broken heart shows that its in alerting state.
Select the master where the signal is to create the alarm
Choose master
Select the port where the signal is to create the alarm
Select port
Select the signal to create the alarm
Select signal
Configure the query
A - Query to apply alarm on
Click on "Options"
Select "Time Range" to measure in, then insert desired "From" value, e.g. now-10s
Set time range
B & C - Remove Reduce and Threshold
Click on delete icon of B Reduce and C ThresholdRemove B & C
Add Classic condition
Click on Add expression
Then click on Classic conditionClassic condition
Configure query in Classic conditionClassic condition query
Set as alert condition
Click on Set as alert condition button
Set as alert condition
Verify condition with Preview
Click on Preview button
Preview
Point 3
Add or select any folder name you want
Add or select any evaulation group you want, this group decides how often the alert will be checked, e.g. every 10 seconds it checks the query interval for the condition
Set a "Pending period", this is the time the alarm could be over the threshold, but not alarming right away
Alert
(Optional) Link the alert to a widget.
In point 4, click on button Link dashboard and panelAlert
Select the widget to link the alert to and confirm
Alert
On the dashboard you can see now the alert within the tile (only if the alert was linked to the widget), and if pending or alerting also in the "Alarms" tile Please remember that the dashboard needs refresh set to on to see changes