Set logging intervalΒΆ
Open connected devices
The connected devices are opened via the rail on the left side.

Connected Devices
- Click on the 3 dots to the right of the master. The menu opens.
- Click Set logging interval to open the dialog to set the logging interval

Set Logging Interval Dialog
- Enter the data rate variably between 50 (500) ms and 60 s in the Logging interval field.
Note
You can operate a maximum of one master and the CMTK itself at 50ms. The other masters can be operated with a maximum of 500ms.
Note
A total of 4 GB is available on the system for data retention. If this value is exceeded, the system deletes the oldest data.