Software updateΒΆ
Here you can update the core apps to the latest software version.
You will find it under Settings > Gateway Settings > Software Update
Software Update location
Note
This will only update the core apps. The other apps can be updated in the App Manager
To select a update file, you have to click on the Upload software file button.
Note
The supported file format is ".mender"
upload file
When the file is uploaded, you can start the installation by clicking on the Start Installation button.
start installation
Note
After the update, the device will reboot. This can take up to 5 minutes. The device wont be accessible for this time.