Time settings¶
On this page you can configure the time.
You will find it under Settings > Gateway Settings > Time Settings
Time Settings location
Manual time settings¶
If you like to set the time manually, you have to make sure, that the NTP Server enabled button is turned off.
NTP Server button
After that you can use the Set time from PC button to get the time or enter it manually.
manual time settings
Network time Protocol¶
If you like to get the time from an NTP server, you have to make sure, that the NTP Server enabled button is turned on.
You can add or delete NTP servers or change their order.
Note
You need at least one server and you can have a maximum of four servers.
NTP server settings
You can add a server by clicking Add NTP Server and entering a server link.
add NTP server
Note
The order of the servers is important. The server with the lower number is always preferred. When the first server isn't accessible, the second one will be used.