User Management¶
By default, there are two users available on the system with the following initial passwords:
| User | Initial password |
|---|---|
| admin | CMTK-adm1n |
| user | CMTK-us3r |
Note
The first time you log in with these users, you will be asked to change the passwords. After resetting to factory settings, the passwords mentioned above are valid again.
You can access user management via the general user interface.


The following functions are available to you in the user settings:
- Add new users
- Edit users
- Delete users
- Activate user
- Deactivate user
- Change passwords

Note
For security reasons, all operations, that can lead to increasing of rights are only available after authentification. Deleting users is also available without authentification.

User Roles¶
Three different user roles with corresponding user rights are provided for the rights of the users. The rights of the roles are summarized in the following table.
| Function | Role: User | Role: Expert | Role: Admin |
|---|---|---|---|
| Grafana | read | write | write |
| Time settings | - | read | write |
| IP settings | - | read | write |
| hostname | - | read | write |
| Update | - | - | write |
| Shutdown / Reboot | - | write | write |
| IO-Link & Master settings | - | write | write |
| Restart Initialisation | - | write | write |
| Reset Grafana | - | write | write |
| DB settings | - | write | write |
| Clear Database | - | write | write |
| Export DB | write | write | write |
| Start/Stop Logging | read | write | write |
| E-Mail settings | - | read/write | write |
| MQTT Settings (mqttconfigurator) | - | read | write |
| Certificates | - | read | write |
| Docker | - | write | write |
| edit device (name, …) | - | write | write |
| Help | read | read | read |
| Log | read | read | read |
| Notifications | read | write | write |