Alert indicator
On this page, you can configure your Smartlight using your configured alerts. To install the Alert Indicator, download the APP and install it on the CMTK.
The Alert Indicator can then be found under Settings > Apps > Alert Indicator
Supported Smartlights¶
The Alert Indicator App supports the following smartlights:
| Product Name | Product Code | Device Id |
|---|---|---|
| BNI IOL-802-102-Z036 | BNI0082 | 330247 |
| BNI IOL-802-102-Z037 | BNI0085 | 330248 |
| BNI IOL-801-102-Z036 | BNI0088 | 330249 |
| BNI IOL-801-102-Z037 | BNI008A | 330256 |
| BNI IOL-803-103-R036 | BNI0E0 | 330288 |
| BNI IOL-800-000-Z037 | BNI0087 | 330246 |
| BNI IOL-800-000-Z036 | BNI007T | 330245 |
| BNI IOL-802-000-Z036 | BNI0072 | 330241 |
| BNI IOL-801-000-Z036 | BNI007F | 330242 |
| BNI IOL-802-000-Z036-006 | BNI0081 | 330241 |
| BNI IOL-802-000-Z037 | BNI0083 | 330243 |
| BNI IOL-802-000-Z037-006 | BNI0084 | 330243 |
| BNI IOL-801-000-Z037 | BNI0086 | 330244 |
| BNI IOL-803-102-R036 | BNI00CZ | 330272 |
| BNI IOL-803-102-R036-012 | BNI000EC | 330304 |
| BNI IOL-803-103-R036-012 | BNI00EE | 330320 |
Add new Alarm¶
To add a new alarm, you should press the New Alarm Assignment button:
This will open a dialog. First you have to select a smartlight and decide which mode to use for the output:
To continue, click on Next.
Now you can select an Alarm and select a Color for each state of this alarm.
Note
Main CMTK alarms are all accruing alarms from this CMTK, excluding alarms from configured node CMTKs.
Note
All Grafana alarms that are created in the CMTK can be used. They are visible at the latest after the first evaluation by Grafana.
Note
If you selected Segmented Alarm in the first step, you can assign the colors to specific segments of the smartlight. If you selected Single Alarm the whole smartlight will have the same color.
In the last step, you get a summary and you can enter a Name for the alarm.
Note
If you want to change the settings before finishing, you can click on Back and adjust them.
If you click on Finish, the alarm will be saved.
When the alarm is saved, a message will be displayed and the alarm is now visible in the table.
Edit Alarm¶
If you want to edit an existing alarm, press the Edit button:
The dialog will be opened with the current settings. You can change the desired settings and after that save with the Finish button.
Delete Alarm¶
To delete an alarm, press the delete button:
To finish the deletion, you need to confirm it:
When the deletion is finished, this message will be displayed: