Radar Sensor Blob UI¶
The Radar Sensor Blob UI visualizes the raw measurement results from the BRS0002 Radar Sensor, making it easier to configure and adjust the sensor.
You can find the app in the main menu under Radar Sensor.
Supported BRS Sensors¶
The Radar Sensor Blob UI app supports the following sensors:
| Product Name | Product Code | Device Id |
|---|---|---|
| BRS S-M30S04-0301-LA2-000S04 (Distance/Object detection) | BRS0002 | 786690 |
| BRS S-M30S04-0301-LA2-000S04 (Radar Reflex Gate) | BRS0002 | 786691 |
Device Selection¶
To begin, select the device you want to visualize. If the device is connected after opening the app, you can refresh the list.
Visualization¶
You can update the visualization manually by clicking Update, or enable Auto Update for automatic refresh.
Different ranges are shown in various colors:
- The Unsafe and Safe Range are set by the sensor’s Measurement Range
(ISDU Index 514). - The Search Window is defined by the Minimum and Maximum distance for target search settings
(ISDU Index 271). - The Threshold is set by the Minimum target strength
(ISDU Index 271).
The Magnitude graph shows what the sensor detects. A higher magnitude means the target is more reflective at that distance.
You can zoom in for a closer look using the controls in the top right corner, or download a screenshot of the graph. To zoom into a specific section, select the area on the graph. To limit the axis range, select the desired range along the axis’s zero line.