Backup and Restore¶
You can create a backup of the CMTK settings which can be used to restore or duplicate the state.
Create a backup¶
You will find the backup settings under Settings > Gateway Settings > General

Click on Create backup and download to open the dialog:

Before downloading, you can decide, if the backup should include the network settings. If you intend to duplicate the settings, this can lead to IP conflicts. It is recommended that you don't back up the network settings if you want to transfer the settings to a new device. If you want to restore the settings to the same device, you can back up the network settings.
Warning
Settings of connected sensors won't be backed up.
Note
The BCM Config Assistant has an option to import and export configuration files of the connected BCMs.
Note
All installed optional apps will also be backed up.
Restore Backup¶
In the settings next to the backup creation, you can also find the backup restoration. Click on Restore from file. Now you can upload the backup file and click on Restore now
Warning
The existing configuration will be overwritten by the backup.
Warning
It's only possible to restore the backup on a device with the same major and minor version.
Information
The device will reboot to restore the backup. Sometimes a refresh is needed after the reboot, because some apps need a little bit more time to start.
Information
Uninstallable apps from the backup are always set to activated in the App Manager. The activation status of the remaining apps is not saved in the backup. Additionally installed apps are not uninstalled after restoration.
Information
For securety reasons, certificates are not backed up and you have to renew them after restoring the backup.

Restore Backup in initialisation¶
After the first login, you can upload a backup as well.