Extension by IO-Link master¶
You can expand the CMTK with additional IO-Link connections by connecting an Ethernet/IP-based IO-Link master.
Supported IO-Link masters¶
The following IO-Link masters are supported:
| Product ID | Product Name |
|---|---|
| BNI006A | BNI EIP-508-105-Z015 |
| BNI009T | BNI EIP-507-005-Z040 |
| BNI00H7 | BNI EIP-508-105-Z067 |
| BNI00HM | BNI EIP-508-005-Z015-013 |
| BNI00HP | BNI XG1-505-0A5-K083 |
| BNI00HR | BNI XG1-505-A05-K084 |
| BNI00K6 | BNI XG5-508-1B5-Z067 |
| BNI00K7 | BNI XG5-538-1B5-Z067 |
| BNI00KH | BNI XG5-508-0B5-R067 |
| BNI00KJ | BNI XG5-538-0B5-R067 |
| BNI00L1 | BNI XG1-505-0A5-R067 |
| BNI00L3 | BNI XG3-508-0B5-R067 |
| BNI00HZ | BNI EIP-508-005-P067 |
Integrate IO-Link master¶
-
Connect the IO-Link master directly to the CMTK via LAN port 1 or LAN port 2 and ensure that the IO-Link master is accessible to the CMTK within the LAN.
Note
IO-Link masters often have a static IP preset at the factory. For connection to LAN port 1 or LAN port 2, this must be adapted, e.g. to Manual within the same IP range.
-
Navigate to the Connected Devices menu and click * Add Master*.

A search is made for reachable IO-Link masters.
Note
Please make sure that the network ports within your network are enabled.

-
Click CONNECT to connect the CMTK to the IO-Link master.The IO-Link master appears under the CMTK.

You can make all other settings as usual for the sensors connected to the IO-Link master. If you want to remove the master again, you will find this setting under the 3 points of the master.
Note
You can add up to 5 masters, one with a maximum logging interval of 50ms and the others with a maximum logging interval of 500ms.