User Management¶
By default, two users are available on the system with the following initial passwords:
| Users | Initial password |
|---|---|
| admin | CMTK-adm1n |
| user | CMTK-us3r |
Note
The first time you login with these users, you will be prompted to change the passwords. After resetting to factory settings, the above passwords are valid again.
You can access the user management via the general user interface.

User settings.
The following functions are available in the user settings:
- Add new users
- Activate user
- Disable user
- Change passwords.
User roles¶
Three different user roles with corresponding user rights are provided for the users configuration. The rights of the roles are summarized in the following table.
| Function | Role: User | Role: Expert | Role: Admin |
|---|---|---|---|
| Grafana | read | write | write |
| Time settings | - | read | write |
| IP settings | - | read | write |
| hostname | - | read | write |
| Update | - | - | write |
| Shutdown / Reboot | - | write | write |
| IO-Link & Master settings | - | write | write |
| Restart initialization | - | write | write |
| Reset Grafana | - | write | write |
| DB settings | - | write | write |
| Clear Database | - | write | write |
| Export DB | write | write | write |
| Start/Stop logging | read | write | write |
| E-mail settings | - | read/write | write |
| MQTT Settings (mqttconfigurator) | - | read | write |
| Certificates | - | read | write |
| Docker | - | write | write |
| edit device (name, ...) | - | write | write |
| Help | read | read | read |
| Log | read | read | read |
| Notifications | read | write | write |