FAQs#
The system is working but I can't see an image#
Note that the radar does not pass through metal/water. In this case, side mounting can help to improve the detection quality.
Where is the radar zone of the radar device?#
| Pos. | Description |
|---|---|
| 1 | Full resolution: 1.75 mm Target width < 262 mm - 2x target distance (mm) |
| 2 | Resolution: 2.8 mm Target width < 262 mm - measuring field distance (mm) |
| 3 | Resolution: 5.2 mm Target width < 262 mm - 0.5x measuring field distance (mm) |
| 4 | Full measuring range |
| 5 | Keep clear: Objects in this area can influence the radar image. |
Settings reset after Restart/Power Outage#
Please be aware that the parameters of the RadarImager are not saved and will require manual reconfiguration after each restart or power outage.
The lack of parameter persistence can have the following implications:
- Configuration Loss: Any customized settings made by the user will be lost, requiring manual reconfiguration after each restart or power outage.
To minimize the impact of parameter loss, we recommend the following:
- Document Parameters: It is advisable to maintain a record of the parameter settings for reference purposes. This will help in quickly restoring the desired configurations after a restart or power outage.