Generate First Image#
Prerequisite
To generate a first image with RadarImager, you need to configure the measurement parameters according to your mounting situation and find the correct layer of interest.
Strategy to generate a first image:
- Step 1: Configure all measurement parameters according to your setup
- Step 2: Generate the first image
- Step 3: Find the correct layer of interest
- Step 4: Optimize the configuration and image quality
Step 1: Configure measurement parameters#
To configure the measurement parameters open the taskMeasurement.measurement.radarSystem
node in the property grid.
Step 1.1: objectSpeedX#
The object speed must be measured with external tools and configured with the objectSpeedX parameter.
For a first image with a visible object, it should be as precise as ±10mm/s.
Tip after generating first image
For a perfect resolution image, optimize the objectSpeedX
parameter to a precision of ±1mm/s.
Step 1.2: objectLengthX and offsetDistanceX#
For a first image configure the parameter objectLengthX to the maximum possible value,
in order to capture the object within the image.
Configure the offsetDistanceX parameter to 0mm
to make sure the object is visible in the image.
Because of the high objectLengthX value, the image might be bigger than required:
Tip after generating first image
Optimize the objectLengthX and offsetDistanceX
parameters to capture the object centered in the most suitable image length.
Step 1.3: distanceZToDeepestLayerOfInterest#
For a first image configure the parameter distanceZToDeepestLayerOfInterest
to the maximum possible value, in order to capture the object within the image stack.
Tip after generating first image
Reduce the distanceZToDeepestLayerOfInterest
parameter as much as possible to ensure maximum performance.
Step 1.4: reverseObjectMovementDirectionX#
If the object is not moving in the default movement direction, enable the
reverseObjectMovementDirectionX parameter to be able to capture the object.
Step 1.5: useExternalTrigger#
Enable the useExternalTrigger parameter to trigger the RadarImager with an external trigger signal.
Tip
Disable the useExternalTrigger
parameter at any time to ensure the currently captured image is not overwritten. Re-enable it to capture a new image.
Step 2: Generate the first image#
After the measurement parameters for the first image are correctly set, you can generate the first image. It is recommended to use a reference object.
Allow the object to pass completely under the RadarImager. The object should trigger an event, and subsequently, the first (blurry) image should be displayed.
Step 3: Find the correct layer of interest#
The RadarImager generates an image stack within the acquisition range, starting from a distance of 10cm. By default, the top layer of the image stack is displayed.
This step describes a strategy for selecting the best layer of the image stack using the imaging parameters in
the taskImaging node.
Step 3.1: globalScale#
By default, each layer is scaled individually.
Enable the globalScale option to scale all layers uniformly.
Tip after generating first image
After finding the layer of interest with the highest reflections,
disable the globalScale
option again to see more details in other layers by scaling them individually.
Step 3.2: layerSelection#
Navigate through the layers step by step by adjusting the layer index with
layerSelection.indexes parameter until the layer with the highest reflections is found.
Congratulations! You have generated the first image with the RadarImager.
Step 4: Optimize the configuration and image quality#
After generating the first image, familiarize yourself with the full parameter guides to achieve the best configuration for your requirements. Additionally, refer to the Optimize Image Quality chapter to improve image quality.