Typical Configuration Errors#
This section shows typical configuration errors and how to recognize them in the images.
Object Movement Direction#
The RadarImager is designed to capture images of objects moving in one direction.
It is possible to select the direction of movement using the objectMovementDirection parameter.
If the object is moving in the wrong direction, the recorded object will be shown by a lot of shadows.
If every second image is displayed incorrectly for an object moving back and forth, the direction-sensitive trigger should be activated so that only images in one direction of movement are recorded.