Impact Control Center User Interface#
The main parts of the user interface are as follows:
Tip
Click on the screenshot to enlarge it.
| Pos. | Description |
|---|---|
| 1 | Drop-down menu with detected devices. |
| 2 | Use button: Reads out the properties of the device and displays them in the property grid. |
| 3 | Update button: Scans the network for compatible GeniCam/GenTL devices |
| 4 | Acquire button: Acquires the 3D images |
| 5 | Image area: Displays the acquired images |
| 6 | Status bar: Displays information about acquisition, for example, the number of frames and error messages. |
| 7 | Property grid to display information about the device and to configure the system for acquisition. |
| 8 | Drop-down menu to select the user experience. This influences the number of properties displayed in the property grid. |