Skip to content

Connecting to RadarImager#

To acquire the first image, you need to establish a connection with the RadarImager, do the Impact Control Center initial configuration and trigger image acquisition with an external trigger sensor connected to Trigger Port1.

Establish connection#

  1. Connect your laptop with the RadarImager via the ethernet connection (RJ45).
  2. Start Impact Control Center.

    Note

    By default, the following warning message appears when you open the application:

    Image title

    Click Yes to continue.

  3. In case that your device is not automatically detected by the application, click Update to scan for compatible GeniCam/GenTL devices:

    Image title

    Once finished, detected GenICam/GenTL devices are available via the drop-down menu at the top left of the toolbar:

    Image title

  4. Click Use to establish connection.

    Image title

Configure Impact Control Center for the initial use.#

The parameters for the device are displayed in the property grid.

  1. On the Settings menu, click Property Grid, and then click Show Property Grid. if the property grid is not yet displayed in a separate pane on the left-hand side:

    Image title

    The property grid displays the basic properties of the selected device.

  2. On the User Experience drop-down menu, select your level of experience (Expert is recommended).

    Image title

    The property grid displays the properties according to your selected user experience:

    Image title

  3. Configure the device according to your needs, and click Acquire.

    An image is acquired and displayed once the RadarImager was triggered on the external Trigger Port1:

    Image title

You have acquired the first image. This image will most likely not be useful for your application, as the RadarImager needs to be configured according to your specific environment and requirements.

Tip

Or refer to the Configuration of RadarImager documentation for detailed information.

To navigate through the layers, see Navigating through the 3D Image Layers.

Enable the Prefer Display Names option#

By default, the parameter names are displayed as follows:

Image title

To improve the readability of the parameter names, select the prefer display names option:

On the Settings menu, click Options and select Prefer Display Names

Image title

The display of the names changes to a more readable format:

Image title