About this guide
Validity
This guide provides all the necessary information for the safe use of the Balluff Network Interfaces with analog inputs and analog outputs. It applies to the following models:
Type |
Order code |
|---|---|
BNI LH1-742-S13-R012 |
BNI00MA |
Read this manual and all related documents completely before installing and operating the product.
This manual was originally created in German. Other language versions are translations of this manual.
© Copyright 2026, Balluff GmbH Zabergäustraße 8, 73765 Neuhausen auf den Fildern
All content is protected by copyright. All rights, including reproduction, publication, editing, and translation, are reserved.
Other applicable documents
Additional information about this product can be found at www.balluff.com on the product page, e.g., in the following documents:
Data sheet
Declaration of conformity
Disposal
Symbols and Conventions
Individual action instructions are indicated by a preceding triangle.
► Instruction
Action sequences are numbered consecutively:
Step 1
Step 2
Numbers unless otherwise indicated are decimals (e.g. 23). Hexadecimal numbers are represented with a preceding 0x (e.g. 0x12AB).
Note, Tip
This info box indicates general notes.
Explanation of the warnings
Always observe the warnings in this guide and the measures described to avoid hazards.
The warnings used here contain various signal words and are structured as follows:
SIGNAL WORD
Type and source of hazard
Consequences if not complied with
► Measures to avert the hazard
The individual signal words mean:
Notice
Identifies a danger that could damage or destroy the product.
Caution
The general warning symbol together with the signal word CAUTION indicates a hazard which can lead to slight or moderate injuries.
Warning
The general warning symbol together with the signal word WARNING indicates a hazard which can lead to death or serious injuries.
Danger
The general warning symbol in conjunction with the signal word DANGER identifies a hazard which, if not avoided, will certainly result in death or serious injury.
Technical terms and abbreviations used
- DPP:
Direct Parameter Page
- EMC:
Electromagnetic Compatibility
- FE:
Function ground
- GND:
Ground
- I/O-Port:
Input/Output Port
- IOL:
IO-Link
- IODD:
Input-Output-Device-Description
- ISDU:
IO-Link-Parameter (Index Service Data Unit)
- LSB:
Least Significant Bit
- MSB:
Most Significant Bit
- PD:
Process Data
- SC:
Short Circuit
- UA:
Actuator supply
- US:
Sensor supply
- CE:
Conformité Européenne, EU conformity marking.
Pictures
Product views and pictures in these operating instructions may differ from the specified product.