Skip to content

Time settings

On this page you can configure the time.
You will find it under Settings > Gateway Settings > Time Settings


Time Settings location

Manual time settings

If you like to set the time manually, you have to make sure, that the NTP Server enabled button is turned off.


NTP Server button

After that you can use the Set time from PC button to get the time or enter it manually.


manual time settings

Network time Protocol

If you like to get the time from an NTP server, you have to make sure, that the NTP Server enabled button is turned on.
You can add or delete NTP servers or change their order.
In addition to NTP, the SNTP protocol is also supported.

Note

You need at least one server and you can have a maximum of four servers.


NTP server settings

You can add a server by clicking Add NTP Server and entering a server link.


add NTP server

Note

The order of the servers is important. The server with the lower number is always preferred. When the first server isn't accessible, the second one will be used.