Skip to content

Commissioning

Commissioning#

Danger

Uncontrolled system movements

During commissioning, and if the radar sensor is part of a control system whose parameters have not yet been set, the system may perform uncontrolled movements. This can endanger people and cause property damage.

  • People must stay away from hazardous areas of the system.
  • Commissioning only by trained personnel.
  • Observe the safety instructions of the system or machine manufacturer.
  1. Check connectors for secure fit and correct polarity. Replace damaged connectors.
  2. Switch on the system.

Electrical connection#

The supply voltage is 15…30 VDC.

For further details, see the IO-Link configuration manual (Link).


Notes on operation#

Caution

High-frequency electromagnetic waves

The antenna of the radar sensor emits high-frequency electromagnetic waves.
To avoid health hazards, additional measures must be taken.

  • Position the antenna so that a safety distance of at least 20 cm between the antenna and workplaces is ensured.
  • Ensure that people do not stay in the immediate vicinity of the antenna for extended periods.

Info

If pin 2 is used as a switching output, the maximum current limitation must be observed (see Technical Data).


Sensor detection ranges#

Blind zone:

  • No object detection takes place in the blind zone. This area should be kept clear for reliable measurements.
  • Objects in the blind zone can cause false reflections and incorrect distance values.
  • Thin materials with low absorption, such as plastic or glass, can be placed and penetrated in the blind zone, e.g., to protect the sensor against mechanical influences. This must be tested individually.
  • In radar reflex-gate mode, depending on the object properties, it is possible to detect objects within the blind zone.

Detection range:

  • Objects are detected if their radar cross-section is sufficient for radar reflections and the alignment is suitable.
  • The maximum range is achieved under the conditions specified in the data sheet.
  • Measurements outside the detection range have not been tested. Use outside the detection range is at your own risk.

Sensor detection ranges

The following standardized target objects are used for radar sensor calibration:

Target object Width/Diameter [m] Depth [m] Radar cross-section [m²] Reflection strength [dB]
Large radar corner reflector (metal) 0.212 0.150 84.82 19.29
Medium radar corner reflector (metal) 0.071 0.050 1.05 0.20
Small radar corner reflector (metal) 0.047 0.033 0.20 -7.02
Metal sphere 0.120 - 0.01 -19.47

Reflectivity and typical radar cross-sections#

Microwaves behave similarly to light due to their small wavelength and show effects such as diffraction, total reflection, mirroring, and interference. These effects are crucial for understanding the properties of radar sensors. An emitted wave is diffusely scattered at an object, with part of the wave being reflected back to the sensor. The strength of this reflection depends on the nature and material of the object.

The radar cross-section indicates how much of the radar signal is reflected by an object back towards the source. It depends on the size, shape, and material of the object. Larger objects with a smooth surface are easier to detect because they have a higher radar cross-section.

A human target has a lower radar cross-section compared to a metal object and is therefore a less effective radar target.

Material dependence

Radar waves propagate unhindered in a vacuum. When they hit an object, the signal changes depending on the nature of the object. Depending on the material, radar waves are completely or partially absorbed or reflected. They can also penetrate various substances.

In summary, absorbing materials are less suitable as radar targets. Although they create a reflection due to the "material jump," most of the radar wave energy is absorbed.

Dielectric Constant

The dielectric constant plays an important role in radar sensors, as it influences the propagation of electromagnetic waves in the material. The dielectric constant is the ratio of the electric field strength in a vacuum to the field strength in the material.

Here are some relevant points:

Material selection

Materials with a high dielectric constant can improve the efficiency of radar sensors by optimizing waveguiding and signal strength.

Signal processing

The dielectric constant influences the reflection and absorption of radar waves, which is crucial for the accuracy and range of the sensors.

Dielectrics (non-conductive materials)

  • With \(\varepsilon_r > 1\), e.g., plastics, glass, paper, ceramics
    • Reflectivity depends on \(\varepsilon_r\)
    • Partial transmission, partial absorption
  • With \(\varepsilon_r >> 1\), e.g., plastics, glass, paper, ceramics
    • Materials with high absorption (e.g., water) can completely absorb radar waves
  • With \(\varepsilon_r \approx 1\), e.g., air, vacuum
    • No attenuation, completely transparent to radar waves

Table with the properties of various materials regarding absorption, reflection, and penetration of radar waves:

Material Absorption Reflection Penetration of Radiation
Metal None Total reflection with direct incidence; refraction and partial reflection possible with oblique incidence None
Wood Medium to strong (depending on moisture content) Low Low
Water Very strong Partial or total reflection possible (depending on angle of incidence) None, due to absorption
Foams Low Low Very low
Plastics Low to high (depending on thickness and type of plastic) Low to high (depending on thickness and type of plastic) Low to high (depending on thickness and type of plastic)
Glass Low to high (depending on thickness of glass) Low to high (depending on thickness of glass) Low to high (depending on thickness of glass)
Clothing Medium to strong (depending on moisture content) Low Low
Rain Low Low Very good
Humans Medium Medium Low
Ice Very high Partial or total reflection possible (depending on angle of incidence) None, due to absorption

Detection range of the radar sensor#

Detection range of the radar sensor


Cleaning#

The radar sensor can be cleaned with a high-pressure cleaner. During cleaning, the radar sensor may not reliably detect a target.

The front cap of the radar sensor can be cleaned with a soft cloth if necessary.


Maintenance#

The product is maintenance-free.