Advanced configuration

This chapter describes various additional features of the EtherCAT Slave. Besides the function description, step-by-step guides on how to configure those features are also included.

Configuring Station Alias

The Station Alias can be selected under the EtherCAT tab, Advanced Settings.

  1. Open ESC Access.

  2. Open E²PROM.

  3. Select Configured Station.

    ../../../../_images/Station_Alias.png

    Configuring Station Alias

Note

The new value is only valid after a reset.

Ethernet over EtherCAT (EoE)

EtherCAT does not transfer any IP packets in normal operation. If IT protocols like MQTT, REST API and OPC UA shall be available when the Network Module is configured to EtherCAT, Ethernet over EtherCAT (EoE) needs to be enabled.

After the successful configuration of EoE the EtherCAT frames will tunnel Ethernet in the EtherCAT protocol thus making it possible to use the IT protocols and WebUI.

Set up

In order to be able to access the web server of the BNI module, access via EoE (Ethernet over EtherCAT) must be configured first.

  1. Select the Advanced Settings… button.

    ../../../../_images/Schaltflaeche_Advanced_Settings.png

    Advanced Settings… button

  2. Enter valid DNS name and valid IP address.

    ../../../../_images/DNS-Name_gueltige_IP.png

    Enter valid DNS name and valid IP address

Preparing network

Before the WebUI or any IT protocols can be reached via EoE, the network of the Beckhoff control must be configured.

Configuring Beckhoff control

A static IP address must be assigned to both network cards.

  1. On the Beckhoff control select Start > Control Panel > Network and dial-up connections > PCI…Settings.

  2. Assign IP address.

    ../../../../_images/IP-Adresse_vergeben.png

    Advanced Settings… button

  3. Under Start > Control Panel > Beckhoff CX Configuration Tool > Miscellaneous activate the setting IP Routing.

    ../../../../_images/IP_Routing_aktivieren.png

    Advanced Settings… button

EoE and PC networks

For the EoE settings in TwinCAT, the IP address of the second network card of the Beckhoff control must be entered as a default gateway.

As a default gateway for the network configuration of the PC, the IP address of the first network card of the Beckhoff control must be entered.

File over EtherCAT (FoE)

File over EtherCAT (FoE) allows transferring files through the EtherCAT protocol to the EtherCAT slave.

The Network Modules use this mechanism to update the device firmware.

Download Firmware File/ Carry out a firmware update

Warning

During active download and installation of the firmware update a continuous power supply needs to be ensured. If power is cut during a firmware update it could damage the device and make it unusable.

For a successful firmware update, the device first needs to be put into Bootstrap state.

  1. Open the Online tab by selecting it.

    ../../../../_images/ethercat-online-marked.png

    Online Tab in TwinCAT

  2. Bring the device into Bootstrap state by clicking the button.

    ⇒ Current State and Requested State show BOOT

    Note

    Bootstrap state can only be switched to if the device is in Init state. Also if the device shall be put into operation mode again it first needs to be switched back into Init.

  3. Select Download in File Access over EtherCAT

  4. Navigate to the folder which holds the firmware file you want to download to the device.

  5. In the extension selection select *.*

    ../../../../_images/selection-dialog-init-marked.png

    File Selection Dialog

    ⇒ The firmware file with extension .bff should now be selectable in the dialog.

  6. Select the desired firmware file and click Open.

  7. In the Edit FoE Filename Dialog no changes are needed. FoE does not require a password. Click on Ok

    ../../../../_images/foe-download-password.png

    Edit FoE Filename Dialog

The firmware will now be downloaded to the device. A running light on the ports indicates the active download and installation. After successful download the device will automatically reboot and boot with the new firmware. Through the CoE object Firmware Build Information the current running version can be inspected and checked if the update was successful.

Connected IO-Link devices can be parameterized in two ways via EtherCAT.

CAN over EtherCAT (CoE)

Via the object 0x4000 (ISDU read/write Ch. X), IO-Link ISDU parameters can be read from or written to the IO-Link device. For this purpose, the corresponding index and subindex must be entered and for writing the corresponding length and data must be entered. The read or write operation is started via the control object. The result is displayed in the status object.

Values for the control

Values for the control

Value

Function

0x00

No function

0x02

Write

0x03

Read

Values for the status

Values for the status

Value

Status

0x00

No status

0x01

Active/Busy

0x02

Access

0x04

Error

0xFF

Fail

Example of CoE setting

This example shows how the index 0x40 of Smartlight (mode) is changed by reading and writing.

  1. Select module.

  2. Open CoE - Online.

  3. Activate the setting Auto Update.

  4. Under Advanced select the setting Online - via SDO Information.

    ../../../../_images/Einstellungen_aktivieren.png

    Activate settings

  5. In port, select 4030:0(here channel 4).

  6. Read index by double clicking 4030:3 and specifying the respective ISDU Index (here 0x0040).

  7. In control write the command 0x03.

    ../../../../_images/Lesen.png

    Read

    ⇒ Content of the index is read and displayed in data.

  8. Change data, specify length and use the command 0x02.

    ../../../../_images/Schreiben.png

    ⇒ The data is written and the parameter is changed in the device.

ADS over EtherCAT Acyclic (AoE)

The ETG.5001.6220 describes AoE instead of CoE for the ISDU read/write access to IO-Link device parameters. Details on ADS can be found in the Beckhoff TwinCAT documentation and in ETG.1020. In contrast to CoE, AoE permits non-blocking processing.

AoE ISDU access uses these definitions (all are 32 bit):

  • AoE IndexGroup = 0x0000F302

  • AoE PortNumber = 0x00001000 + IO-Link port number, starting with 0.

  • AoE IndexOffset

    • 16 Bit IO-Link Index

    • 8 Bit always zero

    • 8 Bit IO-Link Subindex

  • Return error code

    • 16 Bit additional information about the error code, which is 0x0700 (ADS device error).

    • 16 Bit error code via IO-Link

Function blocks ADSREAD and ADSWRITE

../../../../_images/Funktionsbloecke_ADSREAD_und_ADSWRITE.png

Function blocks ADSREAD and ADSWRITE

Function block ADSREAD in TwinCAT

../../../../_images/Funktionsblock_ADSREAD_DE.png

TwinCAT – ADSREAD

ADSREAD commands

Name

Type

Inherited from

Address

Initial

Comment

NETID

T_AmsNetId

–

–

–

AMS NetId

PORT

T_AmsPort

–

–

–

ADS communication port

IDXGRP

UDINT

–

–

–

Index group

IDXOFFS

UDINT

–

–

–

IndexOffset

LEN

UDINT

–

–

–

Maximum number of the data bytes to be read (LEN ≤ maximum size of target buffer)

DESTADDR

PVOID

–

–

–

Pointer to target buffer

READ

BOOL

–

–

–

Rising edge starts command execution.

TMOUT

TIME

–

–

DEFAULT_ADS_TIMEOUT

Maximum permissible time for the execution of this ADS command

BUSY

BOOL

–

–

–

Busy-Flag

ERR

BOOL

–

–

–

Error-Flag

ERRID

UDINT

–

–

–

ADS error code

Function block ADSWRITE in TwinCAT

../../../../_images/Funktionsblock_ADSWRITE_DE.png

TwinCAT – ADSWRITE

ADSWRITE commands

Name

Type

Inherited from

Address

Initial

Comment

NETID

T_AmsNetId

–

–

–

AMS NetId

PORT

T_AmsPort

–

–

–

ADS communication port

IDXGRP

UDINT

–

–

–

Index group

IDXOFFS

UDINT

–

–

–

IndexOffset

LEN

UDINT

–

–

–

Maximum number of the data bytes to be written (LEN ≤ maximum size of source buffer)

SRCADDR

PVOID

–

–

–

Pointer to source buffer

WRITE

BOOL

–

–

–

Rising edge starts command execution.

TMOUT

TIME

–

–

DEFAULT_ADS_TIMEOUT

Maximum permissible time for the execution of this ADS command

BUSY

BOOL

–

–

–

Busy-Flag

ERR

BOOL

–

–

–

Error-Flag

ERRID

UDINT

–

–

–

ADS error code