System commands¶
The device supports various commands that can be accessed via System Commands.
This function is defined in the IO-Link specification and is implemented accordingly.
(see section Reset commands)
| Command Value | Device Action |
|---|---|
| Basic commands | |
| 0x00 (0) | Reserved |
| 0x01 (1) | ParamUploadStart – Starts parameter upload. |
| 0x02 (2) | ParamUploadEnd – Ends parameter upload. |
| 0x03 (3) | ParamDownloadStart – Starts parameter download. |
| 0x04 (4) | ParamDownloadEnd – Ends parameter download. |
| 0x05 (5) | ParamDownloadStore – Finishes parameter setting and starts data storage. |
| 0x06 (6) | ParamBreak – Cancels all Param commands. |
| Switching Channel Teach | |
| 0x40 (64) | Teach Apply – Calculates the switching point for SP1, SP2. |
| 0x41 (65) | Teach SP – Determines teach point 1 for the setpoint and calculates the switching point. |
| 0x41 (65) | Teach SP1 – Determines teach point 1 for setpoint 1 and calculates the switching point. |
| 0x42 (66) | Teach SP2 – Determines teach point 1 for setpoint 2 and calculates the switching point. |
| 0x43 (67) | Teach SP TP1 – Determines teach point 1 for the setpoint 1. |
| 0x44 (68) | Teach SP TP2 – Determines teach point 2 for the setpoint 1. |
| 0x45 (69) | Teach SP2 TP1 – Determines teach point 1 for setpoint 2. |
| 0x46 (70) | Teach SP2 TP2 – Determines teach point 2 for setpoint 2. |
| 0x47 (71) | Teach SP1 Start – Starts dynamic teach-in for setpoint 1 |
| 0x48 (72) | Teach SP1 Stop – Stops dynamic teach-in for the setpoint and calculates the switching point. |
| 0x49 (73) | Teach SP2 Start – Starts dynamic teach-in for setpoint 2 |
| 0x4A (74) | Teach SP2 Stop – Stops dynamic teach-in for setpoint 2 and calculates the switching point. |
| 0x4E (78) | Teach Reset – The teach-in process is interrupted, the setpoints are reset to the default settings. |
| 0x4F (79) | Teach Cancel – The teach-in process is interrupted. |
| Locator | |
| 0x7E (126) | Start Locator |
| 0x7F (127) | Stop Locator |
| General Settings | |
| 0x80 (128) | Device Reset – Device Reset means a warm start of the device. During this process, the microcontrollers are restarted and all initializations performed again without any change made to the parameter values. (see section Reset commands) |
| 0x81 (129) | Application Reset (see section Reset commands) |
| 0x82 (130) | Restore Factory Settings (see section Reset commands) |
| 0x83 (131) | Back-to-Box Reset (see section Reset commands) |
| 0xA5 (165) | Maintenance Reset (see section Reset commands) |
| Balluff Measurement Sensor Profile | |
| 0xE0 (224) | Teach Preset – Sets the current measurement value to the value of Measurement Preset. |
| 0xE1 (225) | Teach Lower Limit – Sets the lower end of the measurement range. |
| 0xE2 (226) | Teach Upper Limit – Sets the upper end of the measurement range. |