Profile Characteristic¶
Description¶
Profile Characteristic is a readable parameter that provides information about which IO-Link profiles are supported. It is used mainly to allow profile function modules of the control unit to detect which profile or functions on the device are available.
This parameter is defined in the IO-Link specification.
ISDU¶
| Name | Index | Subindex | Access | Length | Data Type | Data Storage | Default |
|---|---|---|---|---|---|---|---|
| Profile Characteristic | 0x000D (13) | 0 | R | 14 bytes | UINT16[] | n/a | – |
The parameter can be read via subindex 0 and consists of multiple profile indices and function classes (each 16-bit values).
If a profile ID is specified, this means that all included function classes are supported. If only sub-functions are supported, these are output explicitly as an individual function class.
This device supports the following profiles:
| Profile ID | Name / Description |
|---|---|
| 0x0015 | Measuring and Switching Sensor, high resolution, 2 channel |
| 0x0030 | BLOB transfer |
| 0x0031 | Firmware Update |
| 0x4000 | Common Application Profile: Identification and Diagnosis |
The following function classes are supported:
| Function Class ID | Name / Description |
|---|---|
| 0x8011 | Teach two point extension |
| 0x8012 | Teach dynamic extension |
| 0x8101 | Locator |
All individual functions are described in this guide. For more exact descriptions of the profiles, refer to the corresponding profile specifications (see www.io-link.com).
Variant Dependence¶
There is no variant dependency of profile characteristics