Variant Configuration¶
Description¶
The device variant can be changed either via ISDU with this parameter or by using the IO-Link compatibility mode. If this parameter is written, the device variant is not changed immediately but instead after the device is restarted. If the device variant is changed via the IO-Link compatibility mode, the change in this parameter is visible immediately.
This parameter is not changed by a reset.
The variant dependent functional differences are described in the Radar Frontend section.
ISDU¶
| Name | Index | Subindex | Access | Length | Data Type | Data Storage | Default |
|---|---|---|---|---|---|---|---|
| Device Variant | 0x0055 (85) | 0 | R/W | 2 bytes | UINT16(ENUM) | No | 0x01 |
Device Variant¶
This parameter indicates which variant is currently set.
The following device variants are available:
| Value | Description | Device Id |
|---|---|---|
| 0x01 (1) | Distance/ Object detection | 0x0C0102 (786690) |
| 0x02 (2) | Radar Reflex Gate | 0x0C0103 (786691) |