About this guide
Validity
This guide provides all the information required for the safe use of the BFP 3SA. It applies to the following models: BFP 3SA…
This guide was created in English. Other language versions are translations of this guide.
© Copyright 2026, Balluff GmbH Zabergäustraße 8, 73765 Neuhausen auf den Fildern
All contents are protected by copyright. All rights reserved, including the rights of reproduction, distribution, processing and translation.
Explanation of the warnings
Always observe the warnings in this guide and the measures described to avoid
hazards.
The warnings used here contain various signal words and are structured as
follows:
SIGNAL WORD
Type and source of the hazard
Consequences if not complied with
Measures to avoid hazards
The individual signal words mean:
Notice
Identifies a danger that could damage or destroy the product.
Caution
The general warning symbol together with the signal word CAUTION indicates a hazard which can lead to slight or moderate injuries.
Warning
The general warning symbol together with the signal word WARNING indicates a hazard which can lead to death or serious injuries.
Danger
The general warning symbol in conjunction with the signal word DANGER identifies a hazard which, if not avoided, will certainly result in death or serious injury.
Symbols and conventions
Individual instructions are indicated by a preceding triangle.
Action sequences are numbered consecutively:
Instruction 1
Instruction 2
Numbers unless otherwise indicated are decimals (e.g. 23). Hexadecimal numbers are represented with a preceding 0x (e.g. 0x12AB).
Buttons or selectable menu entries are described in italic and small caps, e.g.Save.
Menu commands are joined with a greater-than sign, e.g. “Settings>Options” stands for the menu command Options from the Settings menu.
Note
Note, tip
This symbol indicates general notes.