Safety notes
Intended use
The model BFP-3SA is a pressure transmitter that is used for pressure measurement in general industrial applications. The instrument may only be used in such applications as are within its technical performance limits, in particular with regard to its material resistance, leakage rate limits and permissible temperature and pressure limits. It is the sole responsibility of the manufacturer or operator of a machine or plant to ensure the suitability of the instrument, and its media resistance, within the application through proper choice of materials and maintenance cycles.
The mounting, dismounting, installation, parameterisation and maintenance of the instrument in industrial environments absolutely requires suitably skilled personnel in accordance with chapter Personnel qualification
The instrument meets the EMC Directive in accordance with EN 61326 for emissions (group 1, class B) and immunity (industrial environment). The instrument has been designed and engineered solely for the intended use described here and may only be used accordingly. The manufacturer shall not be liable for claims of any type based on operation contrary to the intended use.
General safety notes
The instrument described in the operating instructions has been designed and manufactured using state-of-the-art technology. All components are subject to stringent quality and environmental criteria during production. Our management systems are certified in accordance with ISO 9001 and ISO 14001.
These operating instructions contain important information on handling the instrument. Working safely requires that all safety notes and work instructions are observed.
Observe the relevant local accident prevention regulations and general safety regulations for the instrument’s range of use.
The operating instructions are part of the product and must be kept in the immediate vicinity of the instrument and readily accessible to skilled personnel at any time. Pass the operating instructions on to the next operator or owner of the instrument.
Skilled personnel must have carefully read and understood the operating instructions prior to beginning any work.
In this document, the generic masculine is used for better readability. Female and other gender identities are explicitly included.
If available, the provided supplier documentation is also considered to be part of the product in addition to these operating instructions.
The general terms and conditions contained in the sales documentation shall apply.
Subject to technical modifications.
Improper use
Any use beyond or different to the intended use is considered as improper use.
Refrain from unauthorised modifications to the instrument.
Do not use in hazardous areas.
Do not use in safety or emergency shutdown devices.
Do not use in applications with hydrogen.
Do not use in applications with oxygen.
Do not use in places of use that are not protected from weather influences.
Do not use in processes with high condensation.
Do not use in rail vehicles.
Do not use with abrasive and viscous media.
Do not use with medical devices.
Do not use in refrigeration technology.
Personnel qualification
Note
The activities described in these operating instructions may only be carried out by skilled personnel who have the qualifications described below.
Skilled personnel, authorised by the operator, are understood to be personnel who, based on their technical training, knowledge of measurement and control technology and on their experience and knowledge of country-specific regulations, current standards and directives, are capable of carrying out the work described and independently recognising potential hazards.
Warning
Before mounting and commissioning the instrument, ensure you read the operating instructions.