Dismounting, return and disposal

Warning

Physical injuries and damage to property and the environment due to hazardous media Upon contact with hazardous media (e.g. oxygen, acetylene, flammable or toxic substances) and harmful media (e.g. corrosive, toxic,carcinogenic, radioactive), there is a danger of physical injuries and damage to property and the environment. In the event of a fault, hazardous media under high pressure or vacuum may be present at the instrument.

  • For these media, in addition to all standard regulations, the appropriate existing codes or regulations must also be followed.

Dismounting

Only dismount the instrument when it is depressurised and deenergised.

Return

Strictly observe the following when shipping the instrument:

  • All instruments delivered to Balluff must be free from any kind of hazardous substances (acids, bases, solutions, etc.) and must therefore be cleaned before being returned, see chapter Cleaning

  • When returning the instrument, use the original packaging or a suitable transport packaging.

To avoid damage:

  1. Place the instrument in the packaging and evenly pad with shock-absorbent material.

  2. If possible, place a bag, containing a desiccant, inside the packaging.

  3. Label the shipment as transport of a highly sensitive measuring instrument.

Note

Additional information can be found at www.balluff.com on the product page.

Disposal

Incorrect disposal can put the environment at risk. Dispose of instrument components and packaging materials in an environmentally compatible way and in accordance with the country-specific waste disposal regulations.

Disposal of electrical appliances

Do not dispose of with household waste. Ensure a proper disposal in accordance with national regulations.

Do not dispose of with household waste. Ensure a proper disposal in accordance with national regulations.