Overview
>
interfaces
>
Error indications and signals
Error indications and signals
Caution
Physical injuries and damage to property and the environment
If faults cannot be eliminated by means of the measures listed, the flow switch must be removed from the voltage supply immediately.
Ensure that pressure or signal is no longer present and protect against accidental commissioning. If measuring range scaling is set, despite an analog value of 4 mA or 0 V, pressure can still be present.
Contact the manufacturer.
If a return is needed, please follow the instructions given in chapter Return.
Warning
Physical injuries and damage to property and the environment caused by hazardous media
Upon contact with hazardous media (e.g. oxygen, acetylene,flammable or toxic substances), harmful
media (e.g. corrosive, toxic, carcinogenic, radioactive), and also with refrigeration plants and compres
sors, there is a danger of physical injuries and damage to property and the environment.
Should a failure occur, media with extremely high temperature and under high pressure or vacuum may be present at the instrument.
For these media, in addition to all standard regulations, the appropriate existing codes or regulations must also be followed.
Wear the requisite protective equipment.
Note
Additional information can be found at www.balluff.com on the product page.
Faults
In the event of any faults, first check whether the flow switch is mounted correctly, mechanically and electrically.
If complaint is unjustified, the handling costs will be charged.
Faults and corrective measures
Fault
Possible cause
Measure
No output signal
Cable break
Check the continuity
No output signal
No / wrong supply voltage
Rectify the supply voltage
No output signal/cable break
Mechanical load too high
Replace probe with a suitable design
No / wrong output signal
Wiring error
Observe the pin assignment
Wrong output signal
Process temperature out of measuring range;
sensor drift caused by overtemperature
Check temperature range
Wrong output signal
Sensor break/short-circuit
Send the instrument to the manufacturer
Wrong output signal
Sensor drift caused by chemical attack
Check media compatibility
Wrong output signal and too long response time
Wrong mounting geometry, for example mounting depth too small and heat dissipation too high
Move the temperature-sensitive area of the sensor into the medium
Wrong output signal and too long response time
Deposits on the sensor element
Remove deposit
Signal span too small
Supply voltage too high/low
Rectify the power supply
Signal span drops
Moisture has entered
Fit the cable correctly
Warning and errors
Via the digital display, the instrument’s internal errors are displayed. The following table shows the error codes and their
meaning.
Warnings
Warning
Description
ATT1
On changing the switch point, the reset point of the instrument is automatically reduced
ATT2
Trim function cannot be executed because a parameter is outside the permissible limits
For flow unit %: Smallest span for teach function not maintained
For flow units other than %: Offset or correction factor is outside the permissible limit
ATT3
Password entered for menu access is incorrect.
ATT4
The entire measuring range cannot be displayed. DiOL (“display overload”) is shown outside the display range
ATT5
Maximum turndown exceeded.
ILOC
Menu locked over IO-Link.
SC
Short circuit of output 1 or/and output 2
PAS
Prompt for password input.
OL
Overload, measuring range exceeded > approx. 25 % (display blinks)
Errors
Error
Description
ERR
General error
Reset to factory setting
Restart the instrument
ERR1
Ambient conditions outside the specification
Supply voltage too low
Internal temperature at display too high
ERR2
Sensor error
Acknowledgement of an error display by pressing the “Enter” key.