Operation and maintenance

Startup

Danger

Uncontrolled system movement When starting up, if the sensor is part of a closed loop system whose parameters have not yet been set, the system may perform uncontrolled movements. This could result in personal injury and equipment damage.

Please mind the following safety instructions:

  • Persons must keep away from the system’s hazardous zones.

  • Startup must be performed only by trained technical personnel.

  • Observe the safety instructions of the equipment or system manufacturer.

To start up the system, proceed as follows:

  1. Check connections for tightness and correct polarity.

  2. Replace damaged connections.

  3. Turn on the system.

  4. Check measured values and adjustable parameters

Operation Modes

Operation modes

Mode

Description

System start

Digital display is fully activated for 3 s.

When the flow switch is powered up within the range of the hysteresis, the output switch is set to “not active” by default.

Programming mode (setting the parameters)

Activating the programming mode

Keep the “MENU” button pressed for approx. 2 s. If the password is set to≠ 0000, a password will be requested. If authentication is successful, then it enters the programming mode, otherwise it reverts to display mode.

Timeout

If, during the setting of a parameter, no button is pressed for 60 s, the instrument returns to the display mode with the value unchanged.

Display mode (normal operation, display of pressure value)

Returning to display mode

Simultaneous pressing of “INFO” and “MENU”.

Overview of parameters

Overview of parameters

Menu item

Description

Parameter

Factory setting

INI

Initialisation menu

UNIF

Flow unit

m/s, l/min, m³/h, ft/s, ft³/s, US gal/min, Imp. gal/min, %

m/s

TIF

Min/max flow setting, only active when UNIF = %

MIN (NO/YES) sets the current flow value to 0 %; MAX (NO/YES) sets the current flow value to 100 %

0SET

Zero point setting / execution of “Autozero”, only active when UNIF ≠ %

YES / NO; YES sets the current flow value to zero

mu_F

Flow multiplier, only active when UNIF ≠ %

0.10 … 10.00

1.00

uniT

Temperature unit

°C, °F

°C

PIPD

Pipeline diameter in mm, only active when UNIF ≠ %

10 … 1,000

25

SP1 / SP2

Hysteresis function: Switch point (switching output 1, if applicable 2)

0.05 … 3 m/s [0.17 … 9.84 ft/s]; 1.7 … 100 %; if SP2 is configured for temperature: -18.2 … +85 °C [-0.8 … +185 °F]

3.000 m/s

FH1 / FH2

Window function: Window high (switching output 1, if applicable 2)

RP1 / RP2

Hysteresis function: Reset point (switching output 1, if applicable 2)

0 … 2.950 m/s [0 … 9.67 ft/s]; 0 … 98.3 %; if SP2 is configured for temperature: -20 … +78.2 °C [-4 … +172.8 °F]

2.700 m/s

FL1 / FL2

Window function: Window low (switching output 1, if applicable 2)

EF

Extended programming functions

RES

Reset the parameters to factory setting

YES / NO

DS1 / DS2

Switching delay time, which must occur without interruption before any electrical signal change occurs (SP1, if applicable SP2)

0.00 … 65.00 s

0.00 s

DR1 / DR2

Reset delay time, which must occur without interruption before any electrical signal change occurs (RP1, if applicable RP2)

0.00 … 65.00 s

0.00 s

OU1 / OU2

Switching function (switching output 1, if applicable 2)

HNO = hysteresis function, normally open
HNC = hysteresis function, normally closed
FNO = window function, normally open
FNC = window function, normally closed

HNO

OU3

Setting of analog output signal

I = 4 … 20 mA; U = DC 0 … 10 V

I

POL1 / POL2

Switching logic (switching output 1, if applicable 2)

PNP, NPN

PNP

SEL2 / SEL3

Selection for measuring signal of output 2 and, if applicable, output 3

FLOW / TEMP

FLOW

ALOW

Measuring range scaling / turndown (analog value, start value)

Corresponding to analog output

Start of measuring range

AHGH

Measuring range scaling / turndown (analog value, end value)

Corresponding to analog output

End of measuring range

AVGD

Dampening (digital display)

0.00 … 65.00 s

0.20 s

DISM

Display value in display mode

ACT = current flow value; HIGH / LOW = MAX / MIN flow; ACTT = current temperature; OFF = display off

ACT

DISR

Rotate the indication by 180° (digital display)

YES / NO

No

RHL

Clear memory (min/max flow)

YES / NO

PAS

Password entry

0000 = no password; password input digit by digit

0000

TAG

Measuring instrument name (TAG)

32 selectable characters (A–Z, 0–9, -, SPACE). Two consecutive spaces terminate the input and delete this and the subsequent characters.

Without

Certain menu items (light grey) are only displayed if the pressure switch features the respective option

../_images/2026-BFF-3SD_menu_tree.png

Adjustment

Should you wish to adjust the flow switch to local flow conditions, the BFF-3SD offers two ways to make this adjustment.

Adjustment for all units except %

  1. Depressurise the system and switch off the flow.

  2. Mount the flow switch and connect it electrically. see chapter Mechanical mounting and Electrical connection

  3. Select required flow unit in the “INI” menu under “UNIF”.

  4. If there is no flow, select the menu item “0SET” in the “INI” menu, select “YES” and confirm.

  5. Set the flow to a known value in the plant.

  6. Compare this value with the display and calculate the multiplier for the flow value.

Example: System flow velocity: 2.3 m/s
Display FSD-4: 2.5 m/s
muF = 2.3 / 2.5 = 0.92

Enter this value in the initialisation menu under “mu_F” and confirm.
The multiplier function can also be used without prior zero point adjustment.

Adjustment for flow unit %

  1. Depressurise the system and switch off the flow.

  2. Mount the flow switch and connect it electrically.

  3. Recall menu item “SETF” ▶ “MIN” and confirm “0”.

  4. Set the maximum flow in the system.

  5. Recall menu item “SETF” ▶ “MAX” and confirm “100”

Switching functions

Hysteresis function If the flow fluctuates around the set point, the hysteresis keeps the switching status of the outputs stable. With increasing flow velocity, the output switches when reaching the switch point (SP).

  • Normally open contact (HNO): Active

  • Normally closed contact (HNC): Inactive

With the flow decreasing again, the output will not switch back before the reset point (RP) is reached.

  • Normally open contact (HNO): Inactive

  • Contact normally closed (HNC): Active

../_images/BFF-3SD_hysteresis_function.png

Window function

The window function allows for the control of a defined range. When the flow is between window high (FH) and window low (FL), the output switches on.

  • Normally open contact (FNO): Active

  • Normally closed contact (FNC): Inactive When the flow is outside window high (FH) and window low (FL), the output does not switch on.

  • Normally open contact (FNO): Inactive

  • Normally closed contact (FNC): Active

../_images/BFF-3SD_window_function.png

Delay times (0 … 65 s)

This makes it possible to filter out unwanted flow peaks of a short duration or a high frequency (dampening).
The flow value must be present for at least a certain pre-set time for the output to switch on. The output does not immediately change its status when it reaches the switching event (SP), but rather only after the pre-set delay time (DS).

If the switching event is no longer present after the delay time, the switch output does not change.
The output only switches back when the flow has decreased to the reset point (PR) and stays at or below the reset point (RP) for at least the pre-set delay time (DR).

If the switching event is no longer present after the delay time, the switch output does not change

../_images/BFF-3SD_delay_times.png

Dampening function

The time constant “x” specifies the time duration which the digital display, the switching output or the analog signal requires to approach the end value with a deviation of ± 1 % following a change in measured value. After a duration of 2 times “x”, the output value has reached 100 % with a deviation of ± 0.01 % of the prevailing flow.

../_images/BFF-3SD_dampening_function.png

Operating notes

  • Regularly check function of the sensor and all associated components.

  • Regularly check for available firmware and security updates.

  • Regularly review user accounts, access permissions and security-related settings.

  • Take the sensor out of operation whenever there is a malfunction.

  • Secure the system against unauthorized use.

  • Check fasteners and retighten if needed.

Cleaning

Caution

Unsuitable cleaning agents

Cleaning with unsuitable cleaning agents may damage the instrument and the product label.

  • Do not use any aggressive cleaning agents.

  • Do not use any hard or pointed objects.

  • Do not use any abrasive cloths or sponges.

Suitable cleaning agents

  • Water

  • Conventional dishwashing detergent

Cleaning the instrument

  1. Disconnect the flow switch from the mains.

  2. Wipe the instrument surface using a soft, damp cloth.

Maintenance

This flow switch is maintenance-free.