Locator¶
With the Locator function, an IO-Link device can be found again by starting signaling on the LED of the device using a system command. Signaling can be stopped with another system command.
The functionality corresponds to the specification in the IO-Link Common Profile – Locator function class.
ISDU¶
Locator Timeout¶
The Locator Timeout parameter sets the duration of the Locator signal that is displayed via LEDs. The value is specified in minutes. The value range from 1 to 30 minutes is allowed. The parameter is reset by Application Reset and Factory Reset (also see section Reset Commands).
| Name | Index | Subindex | Access | Length | Data Type | Data Storage | Default |
|---|---|---|---|---|---|---|---|
| Locator timeout | 0x00FE (254) | 0 | R/W | 1 byte | UINT8 | Yes | 10 |
System Commands¶
| Command Value | Device Action |
|---|---|
| 0x7E (126) | Start Locator |
| 0x7F (127) | Stop Locator |