Identification¶
The identification data is used for the identification and management of the IO-Link devices.
ISDU¶
| Name | Index | Subindex | Access | Length | Data Type | Data Storage | Default |
|---|---|---|---|---|---|---|---|
| Identification | |||||||
| Vendor Name | 0x0010 (16) | 0 | R | 7 bytes | STRING | n/a | "Balluff" |
| Vendor text | 0x0011 (17) | 0 | R | 15 bytes | STRING | n/a | "www.balluff.com" |
| Variant BRS M30 Premium (Distance/ Object detection) | |||||||
| Product Name | 0x0012 (18) | 0 | R | 55 | STRING | n/a | BRS S-M30S04-0301-LA2-000S04 (Distance/Object detection) |
| Product ID | 0x0013 (19) | 0 | R | 55 | STRING | n/a | BRS S-M30S04-0301-LA2-000S04 (Distance/Object detection) |
| Product text | 0x0014 (20) | 0 | R | 63 | STRING | n/a | Radar sensor Premium, Object Detection & Distance Measurement |
| VariantBRS M30 Premium (Radar Reflex Gate) | |||||||
| Product Name | 0x0012 (18) | 0 | R | 51 | STRING | n/a | BRS S-M30S04-0301-LA2-000S04 (Radar Reflex Gate) |
| Product ID | 0x0013 (19) | 0 | R | 51 | STRING | n/a | BRS S-M30S04-0301-LA2-000S04 (Radar Reflex Gate) |
| Product text | 0x0014 (20) | 0 | R | 43 | STRING | n/a | Radar sensor Premium, Reflex gate mode |
| Serial Number | 0x0015 (21) | 0 | R | 16 bytes | STRING | n/a | |
| Hardware Revision | 0x0016 (22) | 0 | R | 2 bytes | STRING | n/a | |
| Firmware Revision | 0x0017 (23) | 0 | R | ≤ 10 bytes | STRING | n/a | |
| Application Specific Tag | 0x0018 (24) | 0 | R/W | ≤ 32 bytes | STRING | Yes | "***" |
| Function Tag | 0x0019 (25) | 0 | R/W | ≤ 32 bytes | STRING | Yes | "***" |
| Location Tag | 0x001A (26) | 0 | R/W | ≤ 32 bytes | STRING | Yes | "***" |
| Product Type Code | 0x0700 (1792) | 0 | R | ≤ 64 bytes | STRING | n/a | BRS S-M30S04-0301-LA2-000S04 |
| Product Order Code | 0x0701 (1793) | 0 | R | 7 bytes | STRING | n/a | BRS0002 |
Application Specific Tag¶
With the Application Specific Tag parameter, a string (maximum 32 bytes) can be written to the device. This value typically describes the application in which the product is used.
Function Tag¶
With the Function Tag parameter, a string (maximum 32 bytes) can be written to the device. This value typically describes the function of the product in the application area.
Location Tag¶
With the Location Tag parameter, a string (maximum 32 bytes) can be written to the device. This value typically describes the location of the product in the application area.
Product Type Code¶
The Balluff type code is stored permanently in the device.
Product Order Code¶
The Balluff order code is stored permanently in the device.
System Commands¶
For an overview of all System Commands, see section System commands.
Variant Dependence¶
The functionality is available in all variants.