Faults

Caution

Physical injuries and damage to property and the environment

If faults cannot be eliminated by means of the listed measures, the pressure switch must be taken out of operation immediately.

  • Ensure that pressure or signal is no longer present and protect against accidental commissioning.

  • Contact the manufacturer.

  • If a return is needed, please follow the instructions given in chapter Return.

Warning

Physical injuries and damage to property and the environment caused by hazardous media

Upon contact with hazardous media (e.g. oxygen) and also with refrigeration plants and compressors, there is a danger of physical injuries and damage to property and the environment.

  • Should a failure occur, media with extremely high temperature and under high pressure or vacuum may be present at the instrument.

  • For these media, in addition to all standard regulations, the appropriate existing codes or regulations must also be followed.

  • Wear the requisite protective equipment.

Note

Additional information can be found at www.balluff.com on the product page.

In the event of any faults, first check whether the pressure sensor is mounted correctly, mechanically and electrically. If complaint is unjustified, the handling costs will be charged.

Faults and measures

Fault

Possible cause

Measure

No output signal

Cable break

  • Check the continuity

No output signal

No/wrong supply voltage

  • Rectify the supply voltage

No/wrong output signal

Wiring error or switching of switching logic

  • Observe the pin assignment

  • Check the output configuration

Constant output signal upon change in pressure

Mechanical overload caused by overpressure

  • Replace instrument; if it fails repeatedly, contact the manufacturer

Deviating zero point signal

Overload safety exceeded

  • Observe the permissible overload safety

Signal span too small

Mechanical overload caused by overpressure

  • Replace instrument; if it fails repeatedly, contact the manufacturer

Signal span too small

Supply voltage too high/low

  • Rectify the supply voltage

Signal span drops

Moisture has entered

  • Fit the cable correctly