Overview
>
io-link
>
functions-primary
>
Description of the IO-Link functionality
Description of the IO-Link functionality
IO-Link is a point-to-point connection for the communication of the BFP-3SC with
an IO-Link master.
Physical layer
The BFP-3SC supports the following features:
IO-Link features
Property
Value
IO-Link specification
Version 1.1.5
SIO mode
Yes
Minimum cycle time
2.3 ms
Transmission rate
COM2 (38.4 kBaud)
Process data length
16 bit (Frame type 2.2)
Data storage support
Yes
Smart Sensor Profile
Yes
Process Data
The BFP-3SC has 1 digital output. Both physical switching outputs are also transmitted as process data via IO-Link.
In the ‘SIO Mode’ (Standard I/O Mode, without IO-Link operation) the switching output 1 will switch on pin 4 of the M12x1 connector. In the IO-Link communication mode, this pin 4 is reserved exclusively for communication.
With a Frametype 2.2, the 16-bit process data from the pressure switch is transmitted cyclically. Bit 0 is the state of switching output 1, where 1 respectively DC 24 V correspond to the “closed” logic state of the respective output.
The remaining 14 Bit contain the analog value measured by the pressure switch. According to the measuring range of the sensor and the unit configured, the 14 Bit process data of the measured value, is dynamically adjusted. Multiplying the process data with the gradient (Index #67) allows for a pressure reading in the selected unit.
Process data bit allocation
Bit
Process value
Value range
0
OU1
0 = inactive; 1 = active
2–15
ProcessData
-8192 … 8191
Example: Measuring range of the sensor = 0 … 10 psi ProcessData range = 0…1,000 with Gradient = 0.01 In this example: ProcessData 500 = 5.0 psi
Changing the unit, will result in new ProcessData range and Gradient.
Service data (ISDU – Indexed Service Data Unit)
Service data is always acyclic and exchanged on the request of the IO-Link Master. With the help of the service data, the following parameter values or instrument status can be read:
Selection of unit for ProcessData and all related parameters (switch point settings, analogue output scaling, etc.)
67 (0x43)
Gradient
Float32T
4 octets
R
Order-related
Factor for calculation: ProcessData × Gradient = actual pressure in set unit (e.g. ProcessData 0…1000 with gradient 0.01 for 0…10 psi)
68 (0x44)
Start of Measuring Range
IntegerT
2 octets
R
Order-related
Start of measuring range in set ProcessData unit
69 (0x45)
End of Measuring Range
IntegerT
2 octets
R
Order-related
End of measuring range in set ProcessData unit
70 (0x46)
OU1
UIntegerT
1 octet
R/W
HNO
0 = HNO; 1 = HNC; 2 = FNO; 3 = FNC
Switching function – switching output 1
71 (0x47)
DS1
UIntegerT
2 octets
R/W
0
0…65000
Switch delay time switching output 1 [ms]
72 (0x48)
DR1
UIntegerT
2 octets
R/W
0
0…65000
Reset delay time switching output 1 [ms]
73 (0x49)
Damping OU1
UIntegerT
2 octets
R/W
0
0…65000
Damping for switching signal 1 (99%). 0 = no damping active
Output signal settings based on selected unit
Index 66 (0x42) “Unit ProcessData” defines which configurable parameters are
shown in the IO-Link tool and which parameter is prioritized.
(e.g. Index 66 is set to “bar” -> Index 142-145 is shown and can be configured,
any configuration in e.g. Index 202-205 in “psi” will be ignored.)
Switching point parameters (ISDU) index table
Index (dec / hex)
Name
Format
Length
Access
Default value
Value / Range
Remarks
142 (0x8E)
SP1 / FH1_bar
IntegerT
2 octets
R/W
End of measuring range (Start of meas. range + 0.25 %)
End of measuring range (Start of meas. range + 0.25 %) … end of measuring range
Switching point (or window high) value.
The value must always be higher than the reset point (or window low). Minimum gap = 0.25% of pressure range. If Gap < minimum hysteresis, the associated reset point is adjusted automatically.
143 (0x8F)
RP1 / FL1_bar
IntegerT
2 octets
R/W
End of measuring range - 10% of range
Start of meas. range … (end of meas. range - 0.25 %)
Reset point (or window low) value.
The value must always be lower than the switch point (or window high). Minimum gap = 0.25% of pressure range. If Gap < minimum hysteresis, the associated switching point is adjusted automatically.
144 (0x90)
SP2 / FH2_bar
IntegerT
2 octets
R/W
End of measuring range (Start of meas. range + 0.25 %)
End of measuring range (Start of meas. range + 0.25 %) … end of measuring range
See SP1 / FH1; only available for devices with 2 switching outputs.
145 (0x91)
RP2 / FL2_bar
IntegerT
2 octets
R/W
End of measuring range - 10% of range
Start of meas. range … (end of meas. range - 0.25 %)
See RP1 / FL1; only available for devices with 2 switching outputs.
157–160 (0x9D–0xA0)
Index 142 … 145 in Unit “mbar”
IntegerT
2 octets
R/W
See 142 … 145
See 142 … 145
Index 142 … 145 expressed in unit “mbar”
172–175 (0xAC–0xAF)
Index 142 … 145 in Unit “MPa”
IntegerT
2 octets
R/W
See 142 … 145
See 142 … 145
Index 142 … 145 expressed in unit “MPa”
187–190 (0xBB–0xBE)
Index 142 … 145 in Unit “kPa”
IntegerT
2 octets
R/W
See 142 … 145
See 142 … 145
Index 142 … 145 expressed in unit “kPa”
202–205 (0xCA–0xCD)
Index 142 … 145 in Unit “PSI”
IntegerT
2 octets
R/W
See 142 … 145
See 142 … 145
Index 142 … 145 expressed in unit “PSI”
217 to 220(0xD9 to 0xDC)
Index 142 … 145 in Unit “kg_cm²”
IntegerT
2 octets
R/W
See 142 … 145
See 142 … 145
Index 142 … 145 in Unit “kg_cm²”
232 to 235 (0xE8 to 0xEB)
Index 142 … 145 in Unit “%”
IntegerT
2 octets
R/W
See 142 … 145
See 142 … 145
Index 142 … 145 in Unit “%”
Indication
Locate parameter (ISDU)
Index (dec / hex)
Name
Format
Length
Access
Default value
Value / Range
Remarks
106 (0x6A)
Locate me
BooleanT
1 octet
R/W
Off
0 = Off; 1 = On
Helps to locate the device on a machine; flashes the LED indicator in red. “Locate Me” has highest priority (e.g. warnings have lower priority).
Diagnosis
Diagnosis parameters (ISDU)
Index (dec / hex)
Name
Format
Length
Access
Value / Range
Remarks
110 (0x6E)
Temperature Unit
Default value: °C
UIntegerT
1 octet
R/W
0 = °C; 1 = °F
Unit of the internal temperature measurement.
111 (0x6F)
Actual Temperature
Float32T
4 octets
R
Internal temperature measurement of the electronic components.
112 (0x70)
Temperature Low
Float32T
4 octets
R
Minimum temperature since first installation / since “reset low temperature”.
113 (0x71)
Temperature High
Float32T
4 octets
R
Maximum temperature since first installation / since “reset high temperature”.
114 (0x72)
Temperature Low since Power Up
Float32T
4 octets
R
Minimum temperature since last power-up.
115 (0x73)
Temperature High since Power Up
Float32T
4 octets
R
Maximum temperature since last power-up.
120 (0x78)
Pressure Overload Counter
UIntegerT
4 octets
R
Duration in pressure overload range [s].
121 (0x79)
Operating Hours Total
UIntegerT
4 octets
R
Total operating hours since first installation [h].
122 (0x7A)
Operating Hours since Power Up
UIntegerT
4 octets
R
Displays the total operating hours since power-up [h].