Operation and maintenance

Startup

Danger

Uncontrolled system movement When starting up, if the sensor is part of a closed loop system whose parameters have not yet been set, the system may perform uncontrolled movements. This could result in personal injury and equipment damage.

Please mind the following safety instructions:

  • Persons must keep away from the system’s hazardous zones.

  • Startup must be performed only by trained technical personnel.

  • Observe the safety instructions of the equipment or system manufacturer.

To start up the system, proceed as follows:

  1. Check connections for tightness and correct polarity.

  2. Replace damaged connections.

  3. Turn on the system.

  4. Check measured values and adjustable parameters

Operation

Hysteresis function (configurable via IO-Link)

../_images/2026-WIKA_A-1200_hysteresis.png

If the system pressure fluctuates around the set point, the hysteresis keeps the switching status of the outputs stable. With increasing system pressure, the output switches when reaching the switch point (SP).

  • Normally open contact (HNO): Active

  • Normally closed contact (HNC): Inactive

With system pressure falling again, the output will not switch back before the reset point (RP) is reached.

  • Normally open contact (HNO): Inactive

  • Normally closed contact (HNC): Active

Window function (configurable via IO-Link)

../_images/2026-WIKA_A-1200_window_function.png

The window function allows for the control of a defined range. When the system pressure is between window high (FH) and window low (FL), the output switches on.

  • Normally open contact (FNO): Active

  • Normally closed contact (FNC): Inactive

When the system pressure is outside window high (FH) and window low (FL), the output does not switch on.

  • Normally open contact (FNO): Inactive

  • Normally closed contact (FNC): Active

Adjustability:

  • Switch point/Window High The value must be higher than the reset point or window low. The minimum difference is 0.25 % of the measuring range. With a setting less than 0.25 %, the reset point will be adjusted automatically.

  • Reset point/window low The value must be lower than the switch point or window high. The minimum difference is 0.25 % of the measuring range. With a setting less than 0.25 %, the switch point will be adjusted automatically

Delay times (0 … 65 s) (configurable via IO-Link)

../_images/2026-WIKA_A-1200_delay_function.png

This makes it possible to filter out unwanted pressure peaks of a short duration or a high frequency.

The pressure must be present for at least a certain pre-set time for the output to switch on. The output does not immediately change its status when it reaches the switching event (SP), but rather only after the pre-set delay time (DS).

The output only switches back when the system pressure has fallen down to the reset point (PR) and stays at or below the reset point (RP) for at least the pre-set delay time (DR).

If the switching event is no longer present after the delay time, the switch output does not change.

Damping function (0 … 65 s) (configurable via IO-Link)

With this, the time span between a pressure change and the change of the switching state can be set.

Zero point setting

A zero point offset can be reset with the 0SET parameter via IO-Link. Only carry out zero point setting for gauge and vacuum pressure measuring ranges at the start of the measuring range.

Note

Carry out the zero point setting of absolute pressure measuring ranges at 0 bar absolute (vacuum). Since appropriate references are required for this, we recommend that this is only carried out by the manufacturer.

Operating notes

  • Regularly check function of the sensor and all associated components.

  • Regularly check for available firmware and security updates.

  • Regularly review user accounts, access permissions and security-related settings.

  • Take the sensor out of operation whenever there is a malfunction.

  • Secure the system against unauthorized use.

  • Check fasteners and retighten if needed.

Cleaning

Caution

Unsuitable cleaning agents

Cleaning with unsuitable cleaning agents may damage the instrument and the product label.

  • Do not use any aggressive cleaning agents.

  • Do not use any hard or pointed objects.

  • Do not use any abrasive cloths or sponges.

Suitable cleaning agents

  • Water

  • Conventional dishwashing detergent

Cleaning the instrument

Wipe the instrument surface using a soft, damp cloth.

Maintenance

This pressure sensor is maintenance-free.