Safety notes

Intended use

The model BFP-3SC pressure sensor is used for the switching of circuits as a function of the measured pressure via a PNP or NPN output signal. In addition, the pressure value can be output to appropriate read-out units as a standardised digital signal (IO-Link 1.1). The switching conditions can optionally be programmed using IO-Link 1.1 (switch and reset points, switching functions, time response, …).

The model BFP-3SC has been developed for the pressure measurement of non-hazardous fluids, liquids and gases (classification in accordance with Directive 2014/68/EU Article 13, Regulation (EC) No. 1272/2008, or GHS [1] ) which are mainly used for cooling, lubrication, cleaning or power transmission in industrial machines.

Proper function according to the specifications in the technical data is only assured when the product is used solely as described in the user’s guide and the respective documents as well as in compliance with the technical specifications and requirements and only with suitable original Balluff accessories.

Otherwise, there is deemed to be unintended use. Unintended use is not permitted and will result in the loss of warranty and liability claims against the manufacturer.

Reasonably foreseeable misuse

The product is not intended for the following applications and areas and may not be used there:

  • in safety-oriented applications in which personal safety or the safety of machinery and equipment depends on the device function

  • in explosive atmospheres

  • in areas with food contact

  • for processing personal data in accordance with the GDPR

  • for processing financial transactions

General safety notes

Warning

Physical injuries and damage to property and the environment through exceeding the performance limits

Exceeding the performance limits can destroy the instrument and lead to danger in the end-use application.

▶ Only use the instrument in applications that lie within its technical performance limits.

▶ Any permanent operation in the overload range is not permitted. Above the highest permissible operating pressure, up to the overload limit, the pressure sensor is operating outside its specifica-tion. The overload range is intended to prevent damage to the pressure sensor, as part of a pressure vessel system, during the pressure containment test.

▶ The overload limit must never be exceeded, even when failures occur in the end-use application. Loads above the overload limit can cause irreversible damage, which can lead, for example, to permanent measuring errors.

▶ The manufacturer or operator of the machine or plant in which the product is used must ensure the compatibility of the materials of the wetted parts with the medium used.

▶ The pressure switch should not be used with abrasive or unstable fluids, in particular not with hydrogen.

The (dis-)mounting, installation, parameterisation and maintenance of the model BFP-3SC in industrial environments absolutely requires suitably skilled personnel in accordance with its section below.

Info

  • Pressure surges below the nominal pressure and shorter than 1 ms can cause measuring errors.

  • For applications where pressure spikes can occur, the use of a restrictor is recommended. The restrictor narrows the pressure port to 0.6 mm and thus increases the resistance against pressure spikes.

  • With media that could block the pressure port (e.g. through particles), it is recommended to use a wider pressure port of 6 or 12 mm.

  • It must be ensured that no atomic hydrogen can form in the pressure port of the pressure sensor.

Activities such as installation, connection and startup may only be carried out by qualified personnel.

Qualified personnel are persons whose technical training, cyber security training, knowledge and experience as well as knowledge of the relevant regulations allows them to assess the work assigned to them, recognize possible hazards and take appropriate safety measures.

The operator is responsible for ensuring compliance with local safety regulations, maintaining a safe and cyber-secure operating environment, and taking appropriate measures to ensure that a defect in the product will not result in hazards to persons or equipment. This includes assessing cybersecurity risks and implementing the necessary cybersecurity measures for the operation of the machine.

The product must not be opened, modified or changed. If defects and unresolvable faults occur in the product, take it out of service and secure against unauthorized use.

Inadequate isolation of the product may result in damage and malfunction of the product or in the application due to unauthorized access or modification of data and settings or product availability.

Warning

Before mounting and commissioning the instrument, ensure you read the operating instructions.

Use of accessories and spare parts

It is recommended to use original accessories and original spare parts from Balluff. Using accessories and spare parts from third parties can lead to damage to the instrument or accidents, due to quality defects or other reasons.

Balluff assumes no liability for damage or accidents caused by a malfunction or unsuitability of accessories and spare parts which do not originate from Balluff (e.g. non-compliance with the IP ingress protection of connectors).

No warranty claims can be made which arise due to a malfunction or unsuitability of any accessory or spare part from a third party.