Commissioning

In most applications, the BRS level sensor can be used directly after installation.

  • Perform the adjustment procedure only if interfering contours within the measuring range shall be suppressed or the 0 % level shall be adapted to the application.

Adjustment

The BRS level sensor provides an adjustment function for adapting the sensor to the application. During the adjustment process, interfering contours within the measuring range are suppressed and the 0 % level (4 mA) is defined.

  • Perform the adjustment after installation and alignment of the sensor.

  • Use the supplied magnet and follow the steps below to carry out the adjustment procedure.

  1. Hold the magnet to the marked spot, see the “circle” on the product label.

  2. Output signal = 1 mA

    • The magnet was detected by the instrument

    • Continue to hold the magnet to the marked spot (approx. 10 seconds)

  3. Output signal = 2.5 mA

    • Remove the magnet

    • The adjustment process is being carried out (approx. 5 seconds)

The adjustment process is complete when the output signal jumps to a valid value between 4 … 20 mA.