Dismounting, return and disposal
Dismounting
Only dismount the instrument once it has been depressurised and disconnected from voltage supply.
If necessary, ensure that the vessel has strain relief.
Warning
Physical injury
When dismounting, there is a danger from hazardous media and high pressures.
Observe the information in the material safety data sheet for the corresponding medium.
Disconnect the instrument once the system has been depressurised and has cooled down.
Flush or clean the dismounted instrument (following operation), in order to protect persons and the environment from exposure to residual media.
Warning
Risk of burns
When dismounting, there is a danger of physical injuries due to dangerously hot instrument surfaces.
Ensure that the instrument has cooled down to ambient temperature.
Warning
Physical injuries and damage to property and the environment due to hazardous media
Upon contact with hazardous media (e.g. oxygen, acetylene, flammable or toxic substances) and harmful media (e.g. corrosive, toxic, carcinogenic, radioactive), there is a danger of physical injuries and damage to property and the environment.
Should a failure occur, hazardous media with extreme temperatures (over 55 °C [131 °F]), under high pressure or vacuum may be present at the instrument.
For these media, in addition to all standard regulations, the appropriate existing codes or regulations must also be followed.
Return
Caution
Physical injuries
Residual media can result in a risk to persons.
Carry out the cleaning process in accordance with the manufacturer’s instructions.
Strictly observe the following when shipping the instrument:
All instruments delivered to Balluff must be free from any kind of hazardous substances (acids, bases, solutions, etc.) and must therefore be cleaned before being returned, see chapter Cleaning.
When returning the instrument, use the original packaging or a suitable transport packaging.
To avoid damage:
Wrap the instrument in an anti-static plastic film.
Place the instrument in the packaging and pad it evenly with shock-absorbent material.
If possible, include a bag with desiccant in the packaging.
Label the shipment as transport of a highly sensitive measuring instrument.
Note
Information on returns can be found under the heading “Service” on our local website (return application).
Disposal
Incorrect disposal can put the environment at risk.
Dispose of instrument components and packaging materials in an environmentally compatible way and in accordance with the country-specific waste disposal regulations.
Disposal of electrical appliances
This instrument is labelled in accordance with the EU Waste Electrical and Electronic Equipment (WEEE) directive.
Do not dispose of this instrument with household waste.
Hand in old instruments for environmentally friendly disposal at a designated collection point for the disposal of electrical and electronic equipment.
Ensure proper disposal in accordance with national regulations and observe the currently applicable regulations.