Operation and maintenance

Startup

Danger

Unexpected system reactions During commissioning, incorrect parameterization of the measurement system may lead to unexpected reactions of connected control systems. This may result in property damage or hazardous situations. Please mind the following safety instructions:

  • Commission the device only by qualified personnel.

  • Observe the safety instructions of the machine and plant manufacturer.

  • Keep clear of hazardous machine areas during commissioning.

Danger

Uncontrolled system movements

Uncontrolled system movement

When starting up, if the sensor is part of a closed loop system whose parameters have not yet been set, the system may perform uncontrolled movements. This could result in personal injury and equipment damage.

  • Persons must keep away from the system’s hazardous zones.

  • Startup must be performed only by trained technical personnel.

  • Observe the safety instructions of the equipment or system manufacturer.

  1. Check connections for tightness and correct polarity. Replace damaged connections.

  2. Turn on the system.

  3. Check measured values and adjustable parameters and readjust the BRS if necessary. Check the values over the entire measuring range

Note

  • Check for the correct values, especially after replacing the BRS or after repair by the manufacturer.

Operation

Warning

High-frequency electromagnetic waves

The antenna of the radar sensor emits high-frequency electromagnetic waves. To avoid health hazards, additional measures must be taken.

  • Position the antenna so that a safety distance of at least 20 cm between the antenna and workplaces is ensured.

  • Ensure that people do not stay in the immediate vicinity of the antenna for extended periods.

  • Regularly check function of the BRS and all associated components.

  • Take the BRS out of operation whenever there is a malfunction.

  • Secure the system against unauthorized use.

  • Check fasteners and retighten if needed.

Operating states

../_images/2026-BRS0005_operating_states.png

1

Adjustment, active

2

No target detected

3

Target detected below measuring range

4

Target detected within measuring range

5

Target detected above measuring range

6

Transition area: Target detection not guaranteed

Operation states

Output current

Description

4 … 20 mA

Target detected within the measuring range

21.5 mA

Target detected outside the measuring range (beyond the upper measuring range limit)

3.8 mA

Target detected outside the measuring range (below the lower measuring range limit)

2.5 mA

No target detected

1 mA (< 10 seconds)

Adjustment, active

2.5 mA(< 5 seconds)

Adjustment completed

Sensor detection ranges

Blind zone

The device has a blind zone directly in front of the antenna.

  • Reliable level measurement is not possible within the blind zone.

  • Objects located in the blind zone may cause unwanted reflections and influence the measurement result.

  • Thin materials with low attenuation, such as plastics, may be penetrated by the radar signal.

  • Install the sensor so that the expected measuring range is outside the blind zone.

  • Verify suitability in the specific application.

Measuring range

Level measurement is possible within the specified measuring range of the device.

  • The achievable measuring distance depends on the application conditions and the reflective properties of the target medium.

  • The maximum measuring range specified in the technical data is achieved under defined reference conditions.

  • Tanks, vessel geometry, installations, agitators, foam, buildup and product properties may influence the achievable measuring range.

  • Operation outside the specified measuring range is not recommended.

Note

  • For reliable measurements, ensure that no fixed installations such as ladders, pipes, filling equipment or tank internals are located within the main radar beam whenever possible.

Radar reflectivity of different media

Influence of the measured medium

The performance of radar level measurement depends on the reflective properties of the measured medium and its surroundings.

Radar signals are reflected by the surface of the medium. The strength of the reflected signal depends on factors such as the dielectric constant, surface characteristics, and installation conditions.

Media with stronger reflections generally provide more robust and reliable measurements than media with weaker reflections.

Dielectric constant

The dielectric constant (\(\varepsilon_r\) ) describes how a material interacts with electromagnetic waves. For radar level measurement, the dielectric constant influences the strength of the reflected radar signal. In general:

  • Media with a high dielectric constant produce stronger reflections.

  • Media with a low dielectric constant produce weaker reflections.

  • Weaker reflections may reduce the achievable measuring range and signal quality.

Typical reflectivity of different media

The table below provides general guidance regarding the radar reflectivity of common materials.

Typical reflectivity of different media

Material / Medium

Typical Reflectivity

Metal surface

Very high

Water-based liquids

High

Acids and chemicals

High

Glass

Medium

Plastics

Low to Medium

Oils and hydrocarbons

Medium to low

Dry bulk solids

Application dependent

Foam

Low

The actual measurement performance depends on the individual application and operating conditions.

Penetration of non-metallic materials

Radar signals can penetrate many non-metallic materials. Examples include:

  • plastic

  • glass

  • ceramics

This property may allow measurements through plastic containers or protective covers.



The suitability depends on factors such as:

  • material type

  • wall thickness

  • additives and fillers

  • installation conditions

  • Application-specific testing is recommended.



Factors influencing measurement performance The achievable measuring range and signal quality can be influenced by:

  • dielectric constant of the medium

  • foam formation

  • turbulent surfaces

  • buildup on the antenna

  • tank geometry

  • internal installations such as pipes, agitators or ladders

  • installation position of the sensor

  • For optimum performance, install the sensor so that obstacles are avoided within the main radar beam whenever possible.

Cleaning

Note

Damage to property due to improper cleaning

Improper cleaning may lead to damage to the instrument.

  • Do not use any aggressive cleaning agents.

  • Do not use any hard or pointed objects for cleaning.

  • Do not use any abrasive cloths or sponges.

Note

Damage to property and the environment due to residual media

Residual media at the instrument and in the environment can cause damage to property and the environment.

  • Observe the cleaning instructions.

  1. Before cleaning, correctly disconnect the instrument from the pressure supply, switch it off and disconnect it from the mains.

  2. Clean the instrument with a moist cloth.

  • Do not expose the electrical connections to moisture.

Maintenance

The instrument operates maintenance- and wear-free when used as intended; however, it must be subjected to visual inspection within the context of regular maintenance and included in the vessel pressure test. Repairs must only be carried out by the manufacturer.