Safety notes
Intended use
The BRS G1/2” radar level sensor is used to determine the level of oil- and water-based media as well as solids. The range of use is defined by the technical performance limits and materials. The safe operation of the instrument is only ensured if the BRS G1/2” is used correctly in accordance with the operating instructions and any supplementary instructions.
Note
Important Notes:
The instrument may only be operated in approved countries (see information sheet on conformity and approval) and in accordance with national laws.
Proper function is only guaranteed if the device is used in accordance with the manual, all relevant documents, and the technical specifications. Use only original Balluff accessories.
This instrument is not permitted to be used in hazardous areas.
The instrument has been designed and engineered solely for the intended use described here and may only be used accordingly.
It is assumed that the instrument is handled properly and within its technical specifications.
Observe the technical specifications in these operating instructions, see chapter Technical data.
If the instrument is not handled properly or operated within its technical specifications, take it out of service immediately and have it inspected by authorised Balluff service personnel.
The manufacturer shall not be liable for claims of any type based on operation contrary to the intended use.
Reasonably foreseeable misuse
Uses not listed in the description of intended use are prohibited. Such prohibited uses will void any warranty and liability claims against the manufacturer. Technical or electrical modifications to the product are also not permitted, except for updates.
Any use beyond or different to the intended use is considered as improper use.
Refrain from unauthorised modifications to the instrument.
The device must not be used:
in hazardous areas.
in safety or emergency shutdown devices.
with abrasive and viscous media.
with medical devices.
in applications with direct contact with foodstuffs.
General safety notes
Personnel qualification
Installation, commissioning, maintenance and decommissioning of the device may only be performed by qualified personnel authorised by the system owner. Qualified personnel are persons who, based on their technical training, experience and knowledge of applicable regulations and standards, are capable of carrying out the required work and recognizing potential hazards.
Installation and commissioning
Have installation and commissioning of the device performed only by trained specialists.
Use only the components and replacement parts approved by Balluff GmbH in the device data sheet and/or the device operating manual.
Balluff GmbH accepts no liability for damages resulting from improper use or unauthorized manipulation.
Planning the system
Before you commission the device, please carefully read the device data sheet, the device operating manual and the technical documentation for the device (hereafter referred to as “documentation”), where it exists.
The respective, current documentation associated with the device is available from www.balluff.com.
During installation and operation of the device, observe all safety aspects provided in the documentation.
Failure to comply in part or in whole may result in harm to life, the body or health and in property damage.
Adhere to the specifications for the operating voltage according to the documentation.
Observe the details provided in the documentation for the intended use of the device.
Use the device only with an approved power supply.
Using the system
Incorrect voltages may lead to excessive heat and cause a fire. Incorrect connection of the device may cause machine malfunctions!
Observe the voltages specified in the documentation.
Make certain that power is switched off and that the device is grounded during installation and maintenance work.
Operation and testing The system owner and user are responsible for adhering to locally applicable safety regulations.
In the event of device defects and malfunctions, take the device out of operation and safeguard it against unauthorized use.
Electromagnetic Radiation
When handled properly, this device poses no hazard at a distance of 20 cm or more. At a distance of less than 20 cm, heating of exposed body parts in the field (e.g., fingers) is possible.
Balluff recommends that people with pacemakers and pregnant women do not stay in the immediate vicinity of the device.
Do not operate the device near medical equipment or, without prior approval, near military installations, airports, or radio astronomy facilities.
Personnel qualification
Note
The activities described in these operating instructions may only be carried out by skilled personnel who have the qualifications described below.
Skilled personnel, authorised by the operator, are understood to be personnel who, based on their technical training, knowledge of measurement and control technology and on their experience and knowledge of country-specific regulations, current standards and directives, are capable of carrying out the work described and independently recognising potential hazards.
Warning
Before mounting and commissioning the instrument, ensure you read the operating instructions.
Cybersecurity
To operate the product in a cyber secure environment and to ensure the integrity of data, the following measures must be taken:
Check if the delivered product is an original and unmodified device delivered by Balluff GmbH. For more information, see Placeholder.
Perform a risk analysis with regard to cyber security and, based on the identified risks, plan and implement appropriate security measures for a secure environment for the product.
Only allow network access to the devices from outside to known and trusted devices and authorized users.
Only allow authorized personnel physical access to devices from outside.
Implement an information security management system (ISMS) to manage all information security measures.
Implement a firewall to separate the machine/ plantnetwork from the network outside the plant/ machine (company network, Internet) in order to prevent incoming connections to the product’s network interfaces in particular.
For further information, see:
The device are intended for use at Purdue Level 0 “Field Level / Sensors”.
Use a network secured according to the state of the art.
Note on Purdue Level 0: Purdue Level 0 refers to the lowest level of the Purdue reference architecture for industrial automation systems. This level includes the physical sensors and actuators directly connected to the production environment. Devices at this level are responsible for real-time data acquisition and processing.
Allow access to the devices from outside only for known and trusted devices and authorized users.
Protect the sensor and its interfaces against unauthorized physical access by appropriate measures, such as machine access control or physical barriers.
The sensor does not have a digital interface accessible to the user.