About this guide

Validity

This guide provides all the information required for the safe use of the BFP 3SD. It applies to the following models:

BFP 3SD…

This guide was created in English. Other language versions are translations of this guide.

© Copyright 2026, Balluff GmbH Zabergäustraße 8, 73765 Neuhausen auf den Fildern

All contents are protected by copyright. All rights reserved, including the rights of reproduction, distribution, processing and translation.

Disclaimer

The following description is provided free of charge and is a general application example. The description should support the programming and planning of PLC applications and illustrate possible solutions. The user has no claim to warranty, error correction or updates. In particular, any claims for compensation that could result from the use of this description are excluded. This liability limitation excludes

  • (a) damages due to loss of life, personal injury or harm to health,

  • (b) liability in accordance with the Product Liability Act and -

  • (c) cases of intent.

Prior to implementation in systems and machines, please check whether the description provided here is intended for your application. The use of this free description shall be deemed to imply acceptance of the warranty and liability limitation!

Explanation of the warnings

Always observe the warnings in this guide and the measures described to avoid hazards.
The warnings used here contain various signal words and are structured as follows:

SIGNAL WORD

Type and source of the hazard

Consequences if not complied with

  • Measures to avoid hazards

The individual signal words mean:

Notice

Identifies a danger that could damage or destroy the product.

Caution

The general warning symbol together with the signal word CAUTION indicates a hazard which can lead to slight or moderate injuries.

Warning

The general warning symbol together with the signal word WARNING indicates a hazard which can lead to death or serious injuries.

Danger

The general warning symbol in conjunction with the signal word DANGER identifies a hazard which, if not avoided, will certainly result in death or serious injury.

Symbols and conventions

  • Individual instructions are indicated by a preceding triangle.

Action sequences are numbered consecutively:

  1. Instruction 1

  2. Instruction 2

Numbers unless otherwise indicated are decimals (e.g. 23). Hexadecimal numbers are represented with a preceding 0x (e.g. 0x12AB).

Buttons or selectable menu entries are described in italic and small caps, e.g.Save.

Menu commands are joined with a greater-than sign, e.g. “Settings>Options” stands for the menu command Options from the Settings menu.

Note

Note, tip

This symbol indicates general notes.

Technical terms and abbreviations used

ADT:

Fieldbus Autodetection

BET:

Balluff Engineering Tool

DID:

Device ID

EIP:

EtherNet/IP

I/O:

Input/Output

IOL:

IO-Link

ISDU:

IO-Link Parameter (Index Service Data Unit)

MBT:

Modbus

PLC:

Programmable Logic Controller

PNT:

Profinet

SIO:

Standard IO Mode

VID:

Vendor ID