Overview
>
io-link
>
functions-primary
>
Description of the IO-Link functionality
Description of the IO-Link functionality
IO-Link is a point-to-point connection for the communication of the BFP-3SD with
an IO-Link master.
Physical layer
The BFP-3SD supports the following features:
IO-Link features
Property
Value
IO-Link specification
Version 1.1.5
SIO mode
Yes
Minimum cycle time
2.3 ms
Transmission rate
COM2 (38.4 kBaud)
Process data length
16 bit (Frame type 2.2)
Data storage support
Yes
Smart Sensor Profile
Yes
Process Data
The BFP-3SD has 1 or 2 digital outputs and is optionally available with an 4 …
20 mA or 0 … 10 V analogue output signal. Both physical switching outputs are
also transmitted as process data via IO-Link
In the ‘SIO Mode’ (Standard I/O Mode, without IO-Link operation) the switching
output 1 will switch on pin 4 of the M12x1 connector. In the IO-Link
communication mode, this pin 4 is reserved exclusively for communication.
With a Frametype 2.2, the 16-bit process data from the pressure switch is
transmitted cyclically. Bit 0 is the state of switching output 1 and Bit 1 is
the state of switching output 2, where 1 respectively DC 24 V correspond to the
“closed” logic state of the respective output.
The remaining 14 Bit contain the analogue value measured by the pressure switch.
According to the measuring range of the sensor and the unit configured, the 14
Bit process data of the measured value, is dynamically adjusted. Multiplying the
process data with the gradient (Index #67) allows for a pressure reading in the
selected unit.
Process data bit allocation
Bit
Process value
Value range
0
OU1
0 = inactive
1 = active
1
OU2
0 = inactive
1 = active
2–15
ProcessData
-8192 … 8191
Example: Measuring range of the sensor = 0 … 10 psi ProcessData range
= 0…1,000 with Gradient = 0.01 In this example: ProcessData 500 = 5.0 psi
Changing the unit, will result in new ProcessData range and Gradient.
Service data (ISDU – Indexed Service Data Unit)
Service data is always acyclic and exchanged on the request of the IO-Link
Master. With the help of the service data, the following parameter values or
instrument status can be read:
Corresponds to article number on the product label (P#…).
66 (0x42)
Unit Process Data
UIntegerT
1 octet
R/W
Order-related
0 = bar
1 = mbar
2 = MPa
3 = kPa
4 = PSI
5 = kg/cm²
6 = %
Selection of unit for ProcessData and all related parameters (switch point settings, analogue output scaling, etc.)
67 (0x43)
Gradient
Float32T
4 octets
R
Order-related
Factor for calculation: ProcessData × Gradient = actual pressure in set unit (e.g. ProcessData 0…1000 with gradient 0.01 for 0…10 psi)
68 (0x44)
Start of Measuring Range
IntegerT
2 octets
R
Order-related
Start of measuring range in set ProcessData unit
69 (0x45)
End of Measuring Range
IntegerT
2 octets
R
Order-related
End of measuring range in set ProcessData unit
70 (0x46)
OU1
UIntegerT
1 octet
R/W
HNO
0 = HNO
1 = HNC
2 = FNO
3 = FNC
Switching function – switching output 1
71 (0x47)
DS1
UIntegerT
2 octets
R/W
0
0…65000
Switch delay time switching output 1 [ms]
72 (0x48)
DR1
UIntegerT
2 octets
R/W
0
0…65000
Reset delay time switching output 1 [ms]
73 (0x49)
Damping OU1
UIntegerT
2 octets
R/W
0
0…65000
Damping for switching signal 1 (99%)
0 = no damping active
74 (0x4A)
Polarity OU1
UIntegerT
2 octets
R/W
PNP
0 = PNP
1 = NPN
Output Logic for switching output 1
80 (0x50)
OU2
UIntegerT
1 octet
R/W
HNO
0 = HNO
1 = HNC
2 = FNO
3 = FNC
Switching function – switching output 2 (only for devices with 2 outputs)
81 (0x51)
DS2
UIntegerT
2 octets
R/W
0
0…65000
Switch delay time switching output 2 [ms]
82 (0x52)
DR2
UIntegerT
2 octets
R/W
0
0…65000
Reset delay time switching output 2 [ms]
83 (0x53)
Damping OU2
UIntegerT
2 octets
R/W
0
0…65000
Damping for switching signal 2 (99%). 0 = no damping active
84 (0x54)
Polarity OU2
UIntegerT
2 octets
R/W
PNP
0 = PNP
1 = NPN
Output Logic for switching output 2
90 (0x5A)
OU3 Analogue Output Mode
UIntegerT
1 octet
R/W
4 … 20mA
0 = I / 4 … 20 mA
1 = U / 0 … 10V
Signal setting of the analogue output. Only available for devices with analogue output 4 … 20 mA / 0 … 10 V.
91 (0x5B)
Analogue Output Damping
UIntegerT
2 octets
R/W
0
0…65000
Damping for the analogue output signal 2 (τ = 99%) [ms].
0 = no damping active
Output signal settings based on selected unit
Index 66 (0x42) “Unit ProcessData” defines which configurable parameters are shown in the IO-Link tool and which parameter is prioritized.
(e.g. Index 66 is set to “bar” -> Index 140-145 is shown and can be configured, any configuration in e.g. Index 200-205 in “psi” will be ignored.)
Switching point parameters (ISDU) index table
Index (dec / hex)
Name
Format
Length
Access
Default value
Value / Range
Remarks
140 (0x8C)
Analog Output Start Value_bar
IntegerT
2 octets
R/W
Start of measuring range
Start … end of measuring range
Defines the pressure value for start of analogue output signal (e.g. 10 bar = 4 mA). Only available for devices with analogue output.
141 (0x8D)
Analog Output End Value_bar
IntegerT
2 octets
R/W
End of measuring range
Start … end of measuring range
Defines the pressure value for start of analogue output signal (e.g. 78 bar = 20 mA). Only available for devices with analogue output.
142 (0x8E)
SP1 / FH1_bar
IntegerT
2 octets
R/W
End of measuring range (Start of meas. range + 0.25 %)
(Start of meas. range + 0.25 %) … end of meas. range
Switching point (or window high) value. The value must always be higher than the reset point (or window low). The minimum gap between these two points has a value of 0,25% of pressure range.
If the Gap is lower than the minimum hysteresis, the associate reset point will
automatically be changed to observe the limits.
143 (0x8F)
RP1 / FL1_bar
IntegerT
2 octets
R/W
End of measuring range - 10% of range
Start of meas. range … (end of meas. range - 0.25 %)
Reset point (or window low) value. The value must always be lower than the switch point (or window high). The minimum gap between these two points has a value of 0,25% of pressure range.
If the Gap is lower than the minimum hysteresis, the associate switching point will
automatically be changed to observe the limits.
144 (0x90)
SP2 / FH2_bar
IntegerT
2 octets
R/W
End of measuring range (Start of meas. range + 0.25 %)
(Start of meas. range + 0.25 %) … end of meas. range
See SP1 / FH1; only available for devices with 2 switching outputs.
145 (0x91)
RP2 / FL2_bar
IntegerT
2 octets
R/W
End of measuring range - 10% of range
Start of meas. range … (end of meas. range - 0.25 %)
See RP1 / FL1; only available for devices with 2 switching outputs.