Commissioning
Only use original parts and accessories.
Before you begin
To operate the device in a cybersecure environment, take the following measures before commissioning:
Change default user and add a strong password. Secure the password in a safe location.
Check if the device is running the latest firmware version. If not, update the firmware to the latest version that fits your needs.
Set the brute force protection configuration to values that fit your needs.
Replace the default self-signed certificate with a root certificate that is trusted by your organization. Secure the private key in a safe location.
Post-commissioning measures
In order to maintain a secure environment, take the following measures after commissioning:
Create a backup of the device configuration and store it in a secure location.
Adjustability of zero point
Check the indicated zero point on the digital display during commissioning. Should a zero point offset be displayed as a result of installation, this can be reset in programming mode with the 0SET parameter. Only carry out the setting for gauge and vacuum pressure measuring ranges in a depressurised state.
Note
For absolute pressure measuring ranges, the setting must be carried out at 0 bar absolute (vacuum). Since appropriate references are required for this, we recommend that this is only carried out by the manufacturer.