Decomissioning
Note
Exposure of sensitive data
If the device is not decommissioned properly, sensitive data may be exposed. This can lead to unauthorized access to the device and its data.
Reset the device to factory settings to remove any remaining data and configurations.
Dismounting
Depressurise and de-energise the pressure sensor.
Disconnect the electrical connection.
Unscrew the pressure sensor with a spanner using the spanner flats.
Warning
Physical injuries and damage to property and the environment caused by hazardous media
Upon contact with hazardous media (e.g. oxygen), there is a danger of physical injuries and damage to property and the environment.
Should a failure occur, media with extremely high temperature and under high pressure or vacuum may be present at the instrument.
Wear the requisite protective equipment.
Warning
Risk of burns
During dismounting there is a risk of dangerously hot media escaping. The pressure sensor may have heated up severely due to hot media.
Let the instrument cool down sufficiently before dismounting it.
Wear the requisite protective equipment.
Return
Warning
Physical injuries and damage to property and the environment through residual media Residual media in the dismounted instrument can result in a risk to persons, the environment and equipment.
With hazardous substances, include the material safety data sheet for the corresponding medium.
Clean the instrument, see chapter cleaning.
Strictly observe the following when shipping the instrument:
All instruments delivered to Balluff must be free from any kind of hazardous substances (acids, bases, solutions, etc.) and must therefore be cleaned before being returned.
When returning the instrument, use the original packaging or a suitable transport packaging.
Disposal
Incorrect disposal can put the environment at risk. Dispose of instrument components and packaging materials in an environmentally compatible way and in accordance with the country-specific waste disposal regulations.
Do not dispose of with household waste. Ensure a proper disposal in accordance with national regulations.
Note
Additional information can be found at www.balluff.com on the product page.