Error indications and signals

Caution

Physical injuries and damage to property and the environment

If faults cannot be eliminated by means of the listed measures, the pressure switch must be taken out of operation immediately.

  • Ensure that pressure or signal is no longer present and protect against accidental commissioning.

  • Contact the manufacturer.

  • If a return is needed, please follow the instructions given in chapter Return.

Warning

Physical injuries and damage to property and the environment caused by hazardous media

Upon contact with hazardous media (e.g. oxygen) and also with refrigeration plants and compressors, there is a danger of physical injuries and damage to property and the environment.

  • Should a failure occur, media with extremely high temperature and under high pressure or vacuum may be present at the instrument.

  • For these media, in addition to all standard regulations, the appropriate existing codes or regulations must also be followed.

  • Wear the requisite protective equipment.

Note

Additional information can be found at www.balluff.com on the product page.

Faults

In the event of any faults, first check whether the pressure switch is mounted correctly, mechanically and electrically.

Faults and corrective measures

Fault

Possible cause

Measure

No output signal

Cable break

Check the continuity

No output signal

No / wrong supply voltage

Rectify the supply voltage

No / wrong output signal

Wiring error or wrong switching logic / analogue signal

Observe the pin assignment; check the output configuration

Constant output signal upon change in pressure

Mechanical overload caused by overpressure

Replace instrument; if it fails repeatedly, contact the manufacturer

Deviating zero point signal

Overpressure limit exceeded

Maintain permissible overpressure limit

Signal span too small

Mechanical overload caused by overpressure

Replace instrument; if it fails repeatedly, contact the manufacturer

Signal span too small

Supply voltage too high / low

Rectify the supply voltage

Signal span drops

Moisture has entered

Mount the cable correctly

Signal span drops / too small

Diaphragm damaged (impacts, abrasive/aggressive medium, corrosion at diaphragm/process connection)

Contact manufacturer and replace instrument

Warning and errors

Via the digital display, the instrument’s internal warnings and errors are output. The instrument continues to measure, even when a warning exists. The output signal and the switching outputs are still output. EN The following tablen shows the codes and their meaning.

Warnings

Warning

Description

ATT1

On changing the switch point, the reset point of the instrument is automatically reduced to the smallest hysteresis of 0.25 %.

ATT2

Adjustability of zero point: current pressure is outside the limits.

ATT3

Password entered for menu access is incorrect.

ATT4

Unit cannot be displayed on digital display; previous unit is used.

ATT5

Maximum turndown exceeded.

ILOC

Menu locked over IO-Link.

OL

Overpressure: measuring range exceeded > approx. 3.125 % (digital display flashing).

PAS

Prompt for password input.

UL

Vacuum: below measuring range < approx. 3.125 % (digital display flashing).

Errors

Error

Description

ERR

Internal error (restarting the instrument or resetting to factory settings may help).
The analogue output signals the alarm: ≤ 3.6 mA (4 … 20 mA) or ≥ 11 V (0 … 10 V) in accordance with NAMUR43.
The switching outputs retain their current state (open or closed).

ERR1

Instrument temperature exceeded / too low, or supply voltage too low.
Analogue output remains active but accuracy and maximum analogue value may be restricted (temperature influence or low supply voltage).
The switching outputs retain their current state (open or closed).

ERR2

Sensor defect detected, check whether high overpressure is present (can be detected as sensor defect), if necessary, restart instrument or exchange of instrument is needed.
The analogue output controls the alarm signal ≤ 3.6 mA (4 … 20 mA output signal) or ≥ 11 V (0 … 10 V output signal) in accordance with NAMUR43
The switching outputs keep the current switching state (output open or closed)

SC

Short-circuit detected at switching output 1 or 2
The switching output affected is inactive so long as the short-circuit is present