Commissioning
Parameter settings are necessary. For detailed information, see IO-Link interface reference.
The module must be integrated into the control system. The corresponding IODD file is used for this.
Note
The IODD can be downloaded free of charge from www.balluff.com.
Note
For a detailed description of the interface and the data provided here, see the IO-Link interface reference.
Configure analog display values
The module can be configured to display the measured values in different units. For more information, see Configuration of analog value display.