Port Monitoring
Description
The module offers various diagnostic options, such as wire break detection and short circuit protection.
Wire break detection on analog input ports
Analog input ports configured on the voltage input have wire break detection on Pin 2 and Pin 4.
———-How does this work for the the hub—————————
The wire break detection does not work for a current input. Wire break can be signaled in case of fast changing signals. Signals with an edge steepness of > 750 V/s can cause false wire break signals, therefore wire break detection can be activated or deactivated independently for each port (default: deactivated).
Short circuit or wire break detection on analog output ports
Process Data
Name |
Description |
Direction |
|---|---|---|
Pin 1 short circuit |
Status byte for short circuit of Pin 1 |
Input |
Port status |
Status byte for port status. |
Input |
Process data bits for Pin 1 short circuit
Value |
Meaning |
|---|---|
0 |
No short circuit at Pin 1 |
1 |
Short circuit at Pin 1 |
Process data bits for Port status
Bit |
|||||||
|---|---|---|---|---|---|---|---|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
Status Port 8 |
Status Port 7 |
Status Port 6 |
Status Port 5 |
Status Port 4 |
Status Port 3 |
Status Port 2 |
Status Port 1 |
Value |
Meaning |
|---|---|
0 |
Port has no error |
1 |
Port error |
The following events can generate errors on the port status:
Wire break at Pin 2 / Pin 4 for analog input ports
Overcurrent on analog voltage output
Overvoltage (wire break) on analog current output
Process Data Object serves as a collector object. The detailed cause of the event can be read by the ISDU.
ISDU
Port monitoring
Subindex |
Port |
|---|---|
1 |
Port 1 |
2 |
Port 2 |
3 |
Port 3 |
4 |
Port 4 |
5 |
Port 5 |
6 |
Port 6 |
7 |
Port 7 |
8 |
Port 8 |
Value |
Meaning |
|---|---|
0 |
No short circuit at Pin 1 |
1 |
Short circuit at Pin 1 |
System Commands
Events
The following events can generate errors on the port:
Short circuit at pin 1
Wire break at Pin 2 / Pin 4 - analog inputs
Overload - analog outputs