Device Access Locks
Description
With Device Access Locks, the device can be locked for certain types of configuration access to prevent changes to the parameters.
This functionality is defined in the IO-Link standard and is implemented according to Version IOL Spec Version 1.1.4
ISDU
Name |
Index |
Subindex |
Access |
Length |
Data Type |
Data Storage |
Default |
|---|---|---|---|---|---|---|---|
Device Access Locks |
0x0C (12) |
0 |
R/W |
2 Byte |
UINT16 |
n/a |
0 |
The parameter is accessed via subindex 0. Parameter access can be locked by setting the corresponding bits: